[thread border router][i.mx6ull] otbr-agent is inactive

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

[thread border router][i.mx6ull] otbr-agent is inactive

558 Views
felix1
Contributor IV

Hi,

I follow https://github.com/nxp-imx/meta-matter

"How to setup OpenThread Border Router on the target" to run thread border router on i.mx6ull (customized board, not EVK).

The i.mx6ull board not install WiFi module, so I use ethernet instead.

1) When I run the following command, I got the ipset error.

 

root@imx6ullevk:~# otbr-agent -I wpan0 -B eth1 spinel+hdlc+uart:///dev/ttyACM0 &
[1] 603
root@imx6ullevk:~# ipset v7.15: The set with the given name does not exist
ipset v7.15: The set with the given name does not exist
ipset v7.15: The set with the given name does not exist
ipset v7.15: The set with the given name does not exist
ipset v7.15: The set with the given name does not exist
ipset v7.15: The set with the given name does not exist

 

2) I check otbr-agent status is dead

root@imx6ullevk:~# service otbr-agent status
* otbr-agent.service - OpenThread Border Router Agent
Loaded: loaded (/lib/systemd/system/otbr-agent.service; disabled; preset: disabled)
Active: inactive (dead)

 

Can you help me to fix it?

 

Labels (2)
0 Kudos
Reply
0 Replies