the scenarios of i.MX8QM to boot without authentication

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

the scenarios of i.MX8QM to boot without authentication

557件の閲覧回数
GeekFork
Contributor I

Hi Expert,

 

I want to disable the container authentication in my product. Below are the descriptions in processor's reference manual. There are no more details for this situations in the manual.

 

Can anyone help to explain these situations, or where can I find the explanation for them/

 

Thanks!

 

-------

 

The second container, typically containing the SCU FW, DDR Initialization image, M4

image(s), and the FW image(s) for the Cortex A processing domain, is allowed to execute

in the following life cycles without authentication:

  • Fab
  • Fused With Secrets
  • NXP Closed
  • Partial Field Return
  • Full Field Return
0 件の賞賛
返信
1 返信

530件の閲覧回数
AldoG
NXP TechSupport
NXP TechSupport

Hello,

For this you may refer to the security reference manual, chapter 2.1.4.1.1 Chip Life Cycle

Best regards/Saludos,
Aldo.

0 件の賞賛
返信