the range and the exact value list for 24MHz for MIPI sensor with i.MX6Dual

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

the range and the exact value list for 24MHz for MIPI sensor with i.MX6Dual

Jump to solution
1,329 Views
yuuki
Senior Contributor II

Dear all,

We want to capture a camera image by using MIPI-CSI of i.MX6Dual.

We found the following thread.

https://community.freescale.com/docs/DOC-94312

- Debug steps for customer MIPI sensor.docx

According to this document, 27MHz ref_clock is used.

In Tips, the range and the exact value for 27MHz are listed.

We use 24MHz as ref_clock.

Is there these list for 24MHz?

Best Regards,

Yuuki

Labels (1)
0 Kudos
Reply
1 Solution
1,220 Views
Yuri
NXP Employee
NXP Employee

Hello,

  The mentioned 27MHz clock for MIPI is provided internally.
Please take a look at VIDEO_27M_CLK_ROOT in Figure 18-3 (Clock Tree - Part 2)

of the i.MX6 D/Q RM.

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
1 Reply
1,221 Views
Yuri
NXP Employee
NXP Employee

Hello,

  The mentioned 27MHz clock for MIPI is provided internally.
Please take a look at VIDEO_27M_CLK_ROOT in Figure 18-3 (Clock Tree - Part 2)

of the i.MX6 D/Q RM.

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply