the question about internal ADC reference voltage -- i.mx257

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

the question about internal ADC reference voltage -- i.mx257

ソリューションへジャンプ
1,936件の閲覧回数
王剑翰
Contributor III

We want to use the internal ADC reference voltage but we did not find the related information about the accuracy range and temperature drift characteristics of the internal ADC reference voltage.

I only find "The internal reference is fixed at 2.5 V", but I am not sure the accuracy range.

Could you kindly help me for this question?

ラベル(1)
0 件の賞賛
返信
1 解決策
1,773件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi 王

the internal reference voltage accuracy is 4%

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
5 返答(返信)
1,774件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi 王

the internal reference voltage accuracy is 4%

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信
1,773件の閲覧回数
王剑翰
Contributor III

Hi Igor,

Thank you for your kindly answer.

Is the voltage accuracy ±4%?What is the temperature drift characteristics?

Could you kindly show me the related document?

0 件の賞賛
返信
1,773件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi 王

temperature drift included in that value

~igor

1,773件の閲覧回数
王剑翰
Contributor III

Hi Igor,

Thank you for your kindly answer.

I think these specific should be noted in some document, but I can not find it.

Could you kindly show me the related document?

0 件の賞賛
返信
1,773件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi 王

that value is is from internal documents.

It is not from public documents.

~igor