the issue is we are not getting any voltage from the BGA_IMX287DJM4A

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

the issue is we are not getting any voltage from the BGA_IMX287DJM4A

1,183 Views
cad1
Contributor II

hi,

We made one PCB based on PCIMX287DJM4A processor.

Using evaluation board schematics imx28_evk_revD_sch.pdf document.

we are giving 5V from externally to the VDD5V(on borad).

But the issue is we are not getting any voltage from the BGA.

we are observing below voltages form the BGA as follows:

1)VDD4P2 ___1.98V

2)DCDC_VDDIO___0.9V

3)DCDC_VDDA___1.29V

4)DCDC_VDDD___0.7V 

5)VDD1P5___0.120V

Please check the issue and give your suggestions as soon as possible.

regards,

argus technologies.

Address: Plot No. 38, Phase-III, 2nd Floor, Sri Nagar Colony, Kamalapuri Colony, Hyderabad, Telangana 500073

eng@sysargus.com

cad@sysargus.com

9849342471

Labels (1)
Tags (1)
4 Replies

971 Views
cad1
Contributor II

dear igor,

we have filled hardware checklist xls sheet given by you.

please share your mail id to send the hardware checklist.

thanks and regards,

vinay.

0 Kudos
Reply

971 Views
igorpadykov
NXP Employee
NXP Employee

Hi argus

please check

Hardware Design Checklist for i.MX28 

Application note sharing: Issues often met in i.MX28 application 

AN4199 Using the i.MX28 Power Management Unit and Battery Charger

https://www.nxp.com/docs/en/application-note/AN4199.pdf 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

971 Views
cad1
Contributor II

Dear igor,

 

Thanks for the reply , as per your suggestion we will check and update you.

 

Thanks and regards,

Vinay.

0 Kudos
Reply

971 Views
cad1
Contributor II

Dear igor,

Thanks for the reply , as per your suggestion we will check and update you.

Thanks and regards,

Vinay.

0 Kudos
Reply