the imx28 usb gadget driver in uboot

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

the imx28 usb gadget driver in uboot

903 Views
liuxing
Contributor II

Hi All,

  I download the latest uboot code and try to port it in imx28 platform.The uboot can run successfully now

  I want to enable the fastboot function.However,it shows usb device register error.I'm not sure if the imx28 usb device is supported in uboot.

Labels (2)
0 Kudos
3 Replies

645 Views
igorpadykov
NXP Employee
NXP Employee

Hi xing

this may be posted on uboot mail list

lists.denx.de Mailing Lists 

as nxp does not support i.mx28 in its last linux/uboot releases.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos

645 Views
liuxing
Contributor II

Hi,

   Thanks!

   Do you know Is there any uboot version  can support i.mx28 usb gardget?

   Maybe I can try to port it to the new uboot.

0 Kudos

645 Views
liuxing
Contributor II

The fastboot command shows as follows:

=> fastboot 0
g_dnl_register: failed!, error: -19
exit not allowed from main input shell.

0 Kudos