the imax8 support max raw sensor ? raw 10 bit or raw 16bit?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

the imax8 support max raw sensor ? raw 10 bit or raw 16bit?

1,524 Views
gavin-luo
Contributor I

imax8 support max raw sensor bits? 16bit  or 10 bit

0 Kudos
1 Reply

542 Views
art
NXP Employee
NXP Employee

The i.MX8 series processors do not support parallel camera interface, they only support MIPI-CSI2 interface. On this interface, they support all RAW data formats up to RAW16. The i.MX8M and i.MX8X series processors only support up to RAW14 data formats.


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos