the highest temperature of imx6DL

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

the highest temperature of imx6DL

1,263 次查看
haitaochen
Contributor I

We use IMX6D6AVT10AD .  I want to know the highest temperature that we  can Safe to use.

标签 (1)
标记 (1)
0 项奖励
回复
2 回复数

1,124 次查看
igorpadykov
NXP Employee
NXP Employee

Hi haitao

max. temperature is defined parameters given in Table 6. Operating Ranges

for junction temperature

http://www.nxp.com/docs/en/data-sheet/IMX6DQCEC.pdf 

also please check AN4579  i.MX6 Series Thermal Management Guidelines 

http://www.nxp.com/docs/en/application-note/AN4579.pdf 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

1,124 次查看
haitaochen
Contributor I

hello

   I have a problem. I saw that the  ODT settings (MPODTCTRL). So i want to know if set it to 0x00007 or set it to 0x11117.  Will there be any hidden trouble?

0 项奖励
回复