the highest temperature of imx6DL

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

the highest temperature of imx6DL

788 Views
haitaochen
Contributor I

We use IMX6D6AVT10AD .  I want to know the highest temperature that we  can Safe to use.

Labels (1)
Tags (1)
0 Kudos
Reply
2 Replies

649 Views
igorpadykov
NXP Employee
NXP Employee

Hi haitao

max. temperature is defined parameters given in Table 6. Operating Ranges

for junction temperature

http://www.nxp.com/docs/en/data-sheet/IMX6DQCEC.pdf 

also please check AN4579  i.MX6 Series Thermal Management Guidelines 

http://www.nxp.com/docs/en/application-note/AN4579.pdf 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

649 Views
haitaochen
Contributor I

hello

   I have a problem. I saw that the  ODT settings (MPODTCTRL). So i want to know if set it to 0x00007 or set it to 0x11117.  Will there be any hidden trouble?

0 Kudos
Reply