the file "mx6q_sabreauto_boot_weimnor.h" can't find in u-boot-2009.08,where is it?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

the file "mx6q_sabreauto_boot_weimnor.h" can't find in u-boot-2009.08,where is it?

414 Views
jhduan
Contributor I

I want to start on nor flash.But i don't have the mx6q_sabreauto_boot_weimnor.h file.The source of u-boot-2009.08 which freescale supplied don't contain it.Should you supply it for me.Thank you very much!

Labels (2)
Tags (2)
0 Kudos
1 Reply

366 Views
igorpadykov
NXP Employee
NXP Employee

Hi jinghui

I think it is in ../include/configs and named as

mx6q_sabreauto_weimnor.h

Best regards

chip

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos