the error of the sd with qsb program

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

the error of the sd with qsb program

1,148 次查看
ylw
Contributor II

i designed one design that is full of references to the QSB,.and

one board can boot from sd and works fine,but the other board is

not ok .i uused the external power boxeri to supply the power and

the power is 12v,and i used one dc-dc to make 5v.if not plug the

sd into the socket,the power is 12v,but when plug the sd into the

socket ,the power is down to 5v.and when i plug the sd (no

program) into the socket, the power is 12v and all power of the

imx53 is fine .so i want to know what happens .thanks a lot !

0 项奖励
回复
2 回复数

1,091 次查看
jimmychan
NXP TechSupport
NXP TechSupport

if one board is working fine but the other one is not working well, most likely is a hardware issue. Please double check all the pmic voltage outputs are correct and check the SD part of circuit.

1,091 次查看
ylw
Contributor II

hi ,i guess the problem is MICROSD part of circuit.and if i fix it ok ,i will try to boot the board by sd3.thank you again .

在 2013-01-09 16:23:26,jimmychan <admin@community.freescale.com> 写道:

|

|

|

|

the error of the sd with qsb program

created by jimmychan in i.MX Community - View the full discussion

if one board is working fine but the other one is not working well, most likely is a hardware issue. Please double check all the pmic voltage outputs are correct and check the SD part of circuit.

Reply to this message by replying to this email -or- go to the message on Freescale Community

Start a new discussion in i.MX Community by email or at Freescale Community

|

|