the Linux-based SD card created by Mfgtools (Mfgtools-Rel-4.1.0_130816_MX6Q_UPDATER) works for my old MCIMX6Q-SDB card, but FAILS on two new cards (same type)

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

the Linux-based SD card created by Mfgtools (Mfgtools-Rel-4.1.0_130816_MX6Q_UPDATER) works for my old MCIMX6Q-SDB card, but FAILS on two new cards (same type)

1,856 Views
zxinhui
Contributor I

We created a DEMO SD card using an

board (MCIMX6Q-SDB) we bought about 4-5 months back, and Mfgtools-Rel-

4.1.0_130816_MX6Q_UPDATER. But the SD card could not even

start on the new cards we bought this week (the first one does not work,

so we requested a second one)

For the two new cards, booting procedure fails with message like below: " MMC read: dev # 3, block # 2048, count 8192 ... 8192 blocks read: OK Wrong Image Format for bootm command ERROR: cant get kernel image!  "

We can even create a new SD Card using the new boards, but it

does not run on the new boards. However, it runs on the old board.

All 3 (one old and two new) MCIMX6Q-SDB cards have the same

labels like " (SCH-27516 REV C4, 700-27516 REV B)" .

Labels (2)
1 Reply

1,675 Views
igorpadykov
NXP Employee
NXP Employee

Hi Xinhui

could you try latest mfg tools and demo files

L3.14.28_1.0.0_LINUX_DOCS (REV L3.14.28_1.0.0)

http://www.freescale.com/products/arm-processors/i.mx-applications-processors-based-on-arm-cores/i.m...

IMX6_L3.14.28_MFG_TOOL (REV L3.14.28_1.0.0)

http://www.freescale.com/products/arm-processors/i.mx-applications-processors-based-on-arm-cores/i.m...

pay attention to vbs scripts in mfg tools folder.

Regarding Mfgtools-Rel-4.1.0_130816_MX6Q_UPDATER, one can try to flash images

to eMMC Profile Name:SabreSD-eMMC, refer to attached Linux guide sect.4.4 How to Boot From eMMC4.4,

sect.7.2.2 eMMC4.4 on SDHC4.

One can check processor revisions on boards: revision 1.3 (“D”) devices now shipping.

New part number not software backwards compatible if using HAB or plug-in mode.

In general FSL has return service :Returns and Warranty Information|Freescale

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply