Dear Sir
I refer to the IMX6ULLHDG Rev.0.
It is described in 3.5.1 Swapping data lines as following.
"If byte lane swapping was done, target DDR IC register read value must be transposed according to the data line swapping."
I found the following description in the community.
https://community.nxp.com/message/500248
Q1.
Can I understand that the description of NOTE is TYPO?
Best Regards,
Eishi SHIBUSAWA
已解决! 转到解答。
Hi Eishi
NOTE is not typo, but in practice this case is almost never realized
(that is "DDR IC register read value"). NXP BSPs software does not read from ddr mode
registers. If customer reads back ddr mode register, then he should follow this NOTE.
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Eishi
NOTE is not typo, but in practice this case is almost never realized
(that is "DDR IC register read value"). NXP BSPs software does not read from ddr mode
registers. If customer reads back ddr mode register, then he should follow this NOTE.
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------