supporting Gigabit Ethernet in imx6 board by yocto L4.1.15

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

supporting Gigabit Ethernet in imx6 board by yocto L4.1.15

767 Views
qi908542785
Contributor I

Hi,

We are using a Sabresd board (i.MX6Q) with YOCTO 4.1.15 kernel.On the basis of Sabresd board own development board.

The system default is 100M Ethernet,We want to achieve Gigabit Ethernet.

What need to modify the support Gigabit Ethernet,Hope to get your help.

Regards,

QI.

0 Kudos
Reply
1 Reply

446 Views
igorpadykov
NXP Employee
NXP Employee

Hi

please check rgmii timing with oscilloscope given in

Table 62. RGMII Signal Switching Specifications i.MX6DQ Datasheet

http://cache.freescale.com/files/32bit/doc/data_sheet/IMX6DQCEC.pdf

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply