supported USB Camera moules for i.MX7D / Android N7.1.2_2.0.0

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

supported USB Camera moules for i.MX7D / Android N7.1.2_2.0.0

881 次查看
eric_kang
Contributor II

Dear All,

I'm finding the USB Camera module for i.MX7D / Android N7.1.2_2.0.0.

I confirmed the below USB Cameras were supported in i.MX7D / Android N7.1.2_2.0.0.

Logitech C250 / C920 / E3500

But those cameras couldn't apply to our boards, because the cameras are a stand-alone USB type Camera, not module.

So we have to find the module type USB Camera.

Please tell me if you know the camera module.

Best Regards,
Eric.

标签 (3)
0 项奖励
回复
1 回复

518 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Eric

I have internal confirmation that usb camera is not supported on MX7D.

The release note will be updated.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复