Hi,
I need to perform calibration for the iMX6DQP SoC however,
There is no MX6DQP option in the NXP DDR Test Tool V2.80.
Is calibration for the MX6DQP supported in this version?
Should calibration for the i.Mx6DQP be done by selecting MX6DQ in TARGET field?
Aviad
Hello Ofer Austerlitz,
You can use the i.MX6DQ option on the DDR Stress Tool. However, you would need the i.MX6QP script file, which you can generate with the script aid below (which you probably already have):
https://community.nxp.com/docs/DOC-331930
I hope this helps!
Regards,