strange pop using sgtl5000

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

strange pop using sgtl5000

1,293件の閲覧回数
ieio
Contributor IV

Hi I am using sgtl5000 on a, imx6 based custom board, and  its alsa driver included in LTIB.

Randomly I hear a pop after I played a WAV, doesn't matter if I play it using aplay or my application.

I always keep Bias ON (echo 1 >/sys/devices/platform/soc-audio.1/HiFi/bias_always_on) to avoid any potential noise due to some mistakes in setting the bits in the CHIP_ANA_POWER register in the right sequence.sgtl5000.jpeg.jpg

As you can see from the image, on LINEOUT there is a negative spike (the pop I hear) after the tone I play.

As I said this spike is apparently random, most of the time the signal is correct and sound clean.

Anyone has some clues about the cause of this behavior?

Thanks in advance,

i.

ラベル(2)
0 件の賞賛
返信
0 返答(返信)