Hi Guys,
I have a imx6s custom board. i Got the task to add customized uboot support with LPDDR2. i have already followed imx6 BSP development pdf. but coming to ddr configuration i have issues. What i'm looking for is the in depth modification of uboot because i have git clone uboot_2014.01 from git repository with respect to imx6 board. this uboot doesn't have imx6s support. so i have referred imx6 duallite. if some one has done for imx6s can you share me some information.
1-> What are the basic peripheral information needed?
like UART support, SD card support,LPDDR2 DCD fillup?
2-> step by step what are the changes to be made in uboot ?
i have used imx6dqsdl script to generate ddr register values but their also i have issue. i'm using micron MT42L128M32D1LF. Please check once micron pdf with respect to below value is it correct or not.
| Device Information | |
| Manufacturer: | Micron |
| Memory part number: | MT42L128M32D1LF-18 |
| Memory type: | LPDDR2-800 |
| DRAM single die density (Gb) | 4 |
| DRAM density per Channel (Gb) | 4 |
| DRAM Bus Width | 32 |
| Number of Chip Selects used per Channel | 1 |
| DRAM density per CS (Gb) | 4 |
| DRAM Bus Width Per Channel | 32 |
| Number of Banks | 8 |
| Number of ROW Addresses | 14 |
| Number of COLUMN Addresses | 10 |
| System Information | |
| i.Mx Part | i.Mx6S |
| MMDC channels: | MMDC0 |
| Bus Width | 32 |
| DRAM Clock Freq (MHz) | 400 |
| DRAM Clock Cycle Time (ns) | 2.5 |
| 4KB Interleaving Mode | Non-Interleave |
| SI Configuration | |
| DRAM DSE Setting - DQ/DQM (ohm) | 40 |
| DRAM DSE Setting - ADDR/CMD/CTL (ohm) | 40 |
| DRAM DSE Setting - CK (ohm) | 40 |
| DRAM DSE Setting - DQS (ohm) | 40 |
one more thing so far i have not lpddr2 stress test in uboot for calibration. because i uboot shell is not prompting so i thought it's better to take step by step fully understand where and what i'm missing.
Hi,
You can find a document named "i.MX_6_BSP_Porting_Guide.pdf" in the document package downloaded from freescale website. It is EXACTLY what you need to do to finish your works. Well prepared documents, just follow it and ...done!
Good luck!
davidtrinh In my post i have clearly mention i have followed every step of BSP porting but still i'm not getting any clarity. please check once again my post i have pointed out some questions? if will be very helpful if you help me out