spi_mx_200c000.ecspi:dma setup error -19, use pio

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

spi_mx_200c000.ecspi:dma setup error -19, use pio

1,767 Views
surendradhobale
Contributor III

Hello,

      In our imx6ul based custom board, we are using the spi-uart bridge expander (max4830).

I am able to probe on the spi bus.

but in the kernel logs, received logs like,

spi_mx_200c000.ecspi:dma setup error -19, use pio

spi_imx_2008000.ecspi probed.

on MAX14830 expander, able to read revision id of the chip.and able to open the ports (/dev/ttyMAX0, /dev/ttyMAX1)

I am doing the loopback test, reception of the data getting correctly. But after some time ( say 3 -4 min) ports becomes hang or communiaction stops. If we exit from the port and restart the same port again,then no communication happend.

After reboot of the board and communication happens but for littel time.

Doesnot understand the problem ?

(spi_mx_200c000.ecspi:dma setup error -19, use pio) what is this error

what could be the problem in such issue of stop communication after some time.

(I have checked this on the kernel 4.1.15 and 4.9 also on both kernel same observation.)

Thanks in advance !!!

Labels (3)
0 Kudos
Reply
1 Reply

1,427 Views
jimmychan
NXP TechSupport
NXP TechSupport

what is your device tree setting for this spi

0 Kudos
Reply