spi driver can not receive

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

spi driver can not receive

Jump to solution
1,947 Views
pensive
Contributor I

imx53   L2.6.35_11.09.01 linux-2.6.35.3

if I use transport test , I can transport buf to spi slave,

transport test:

st[ 1 ].tx_buf = buf;

st[ 1 ].len =1;

but when I use receive test, I can receive any message, the spi bus is always 0x80.when I insmod module,the system is crash and print cann't use tx_buf  = NULL .

receive test:

st[ 1 ].rx_buf = buf;

st[ 1 ].len =1;

setup spi :

8bit/w 15000000kbps

also I cann't find "mxc_spi_buf_tx_u8" in my linux code.

kernel print:

[fkuexl]#insmod ads7846.ko

ads7846 probe start

mxc_spi_setup: mode 0, 8 bpw, 1500000 hz

setup mode 0, 8 bits/w, 1500000 Hz max --> 0

ads7846 spi2.0: touchscreen, irq 128

spi_sync 111

xfer_len=8 master_drv_data->usedma=1

mxc_spi_pio_transfer tx=cf325800,rx=0,len=1

transfer.count =1

transfer.rx_count=1

spi_sync 222=0

clk

transfer.count=0

mxc_spi_pio_transfer tx=0,rx=cf325804,len=2

transfer.count =2

transfer.rx_count=2

Unable to handle kernel NULL pointer dereference at virtual address 00000000

pgd = 80004000

[00000000] *pgd=00000000

Internal error: Oops: 17 [#1] PREEMPT

last sysfs file: /sys/devices/virtual/gsl_kmod/gsl_kmod/dev

Modules linked in: ads7846(+)

CPU: 0    Not tainted  (2.6.35.3-1129-g691c08a-fkuexl #255)

PC is at mxc_spi_buf_tx_u8+0x8/0x14

LR is at mxc_spi_pio_transfer+0x110/0x1ec

pc : [<802d64a8>]    lr : [<802d74f8>]    psr: 80000013

sp : cf0a3f20  ip : d0936000  fp : d0876004

r10: 00000001  r9 : d0876000  r8 : 00000002

r7 : 00000000  r6 : cf0f3518  r5 : cf0f3600  r4 : cf325858

r3 : 00000000  r2 : cf0f3518  r1 : 807f91fa  r0 : cf0f3518

Flags: Nzcv  IRQs on  FIQs on  Mode SVC_32  ISA ARM  Segment kernel

Control: 10c5387d  Table: bf3bc019  DAC: 00000017

Process mxc_spi.1 (pid: 225, stack limit = 0xcf0a22e8)

Stack: (0xcf0a3f20 to 0xcf0a4000)

3f20: 802d73e8 cf0f3600 cf325858 cf0a2000 cf325828 cf325808 cf0f3600 cf0f3518

3f40: 00000000 802d6594 cf325858 00000000 cf0a2000 802d49e0 cf0a2000 ffffffff

3f60: 802d6564 cf0f352c cf0e4cc0 cf0a2000 cf0e4cc0 cf0e4cc8 802d4870 cf0a3f94

3f80: cf0f3520 00000000 cf0f351c 800c0248 cf0a2000 00000000 cf1b65c0 800c3b10

3fa0: cf0a3fa0 cf0a3fa0 00000000 cf039e78 cf0a3fd4 800c00cc cf0e4cc0 00000000

3fc0: 00000000 00000000 00000000 800c37dc 00000000 00000000 cf0a3fd8 cf0a3fd8

3fe0: 00000000 cf039e78 800c3764 800899c0 00000013 800899c0 5a999cc1 5a899cc9

[<802d64a8>] (mxc_spi_buf_tx_u8+0x8/0x14) from [<802d74f8>] (mxc_spi_pio_transfer+0x110/0x1ec)

[<802d74f8>] (mxc_spi_pio_transfer+0x110/0x1ec) from [<802d6594>] (mxc_spi_transfer+0x24/0x28)

[<802d6594>] (mxc_spi_transfer+0x24/0x28) from [<802d49e0>] (bitbang_work+0x170/0x2e0)

[<802d49e0>] (bitbang_work+0x170/0x2e0) from [<800c0248>] (worker_thread+0x17c/0x228)

[<800c0248>] (worker_thread+0x17c/0x228) from [<800c37dc>] (kthread+0x78/0x80)

[<800c37dc>] (kthread+0x78/0x80) from [<800899c0>] (kernel_thread_exit+0x0/0x8)

Labels (1)
Tags (2)
0 Kudos
1 Solution
1,193 Views
zhaozhao
Contributor III

Hi ,

You can try to modify drivers/spi/mxc_spi.c. Change the MXC_SPI_BUF_TX(type) as below. Hope this helps.

#define MXC_SPI_BUF_RX(type)    \
void mxc_spi_buf_rx_##type(struct mxc_spi *master_drv_data, u32 val)\
{\
    type *rx = master_drv_data->transfer.rx_buf;\
    if(rx) {    \
        *rx++ = (type)val;\
        master_drv_data->transfer.rx_buf = rx;\
    }   \
}

#define MXC_SPI_BUF_TX(type)    \
u32 mxc_spi_buf_tx_##type(struct mxc_spi *master_drv_data)\
{\
    u32 val;\
    const type *tx = master_drv_data->transfer.tx_buf;\
    if(tx) {    \
        val = *tx++;\
        master_drv_data->transfer.tx_buf = tx;\
        return val;\
    }   \
    master_drv_data->transfer.count -= sizeof(type);\
    return 0;\
}

View solution in original post

0 Kudos
6 Replies
1,193 Views
fabio_estevam
NXP Employee
NXP Employee

You forgot to mention the FSL processor you are using, BSP version, etc :-)

0 Kudos
1,193 Views
pensive
Contributor I

I have update some informations.can you help me?

0 Kudos
1,193 Views
zhaozhao
Contributor III

Hi,

     I found that the spi could not work normally when i modified the file as above. Try to port drivers/spi/spi_imx.c to your current kernel from a higher version of kernel, such as linux-3.0.35.

Sorry for the mistake.

0 Kudos
1,193 Views
ricardo_ioct
Contributor III

Hi,

I'm with the same issue with the SPI on i.MX53. On my BSP, I have the spi_imx module ported, but, when I probe it, the inode /dev/spixxx isn't created. Do you have more hints about the usage of spi_imx on kernel 2.6.35?

0 Kudos
1,193 Views
zhaozhao
Contributor III

Hi ,

     I'm using imx51. I ported the spi_imx from linux-3.0.35(the kernel for imx6) to kernel 2.6.35. There is no /dev/sipXX, but I can operate through SPI normally in the driver layer.

0 Kudos
1,194 Views
zhaozhao
Contributor III

Hi ,

You can try to modify drivers/spi/mxc_spi.c. Change the MXC_SPI_BUF_TX(type) as below. Hope this helps.

#define MXC_SPI_BUF_RX(type)    \
void mxc_spi_buf_rx_##type(struct mxc_spi *master_drv_data, u32 val)\
{\
    type *rx = master_drv_data->transfer.rx_buf;\
    if(rx) {    \
        *rx++ = (type)val;\
        master_drv_data->transfer.rx_buf = rx;\
    }   \
}

#define MXC_SPI_BUF_TX(type)    \
u32 mxc_spi_buf_tx_##type(struct mxc_spi *master_drv_data)\
{\
    u32 val;\
    const type *tx = master_drv_data->transfer.tx_buf;\
    if(tx) {    \
        val = *tx++;\
        master_drv_data->transfer.tx_buf = tx;\
        return val;\
    }   \
    master_drv_data->transfer.count -= sizeof(type);\
    return 0;\
}

0 Kudos