something wrong with 1080P on IMX535

cancel
Showing results forย 
Search instead forย 
Did you mean:ย 

something wrong with 1080P on IMX535

172 Views
leeo
Contributor I

I have heared that many people say lvds can't output 1080P, when I try to  check source code ,

If i set the mode is "Spilt",
the code will set the  pixclk is 2*455/7=120M pixclk/s,

check as double rate ,it will be 240M, It will be larger than the width 1080P needed.

when I set to splite mode,fb0 shows

cat mode:

U:1920*1080P-56

but  I can't  measure the clk on the pin...so I can't understand it ,so strangely.

Labels (1)
0 Kudos
2 Replies

40 Views
igorpadykov
NXP TechSupport
NXP TechSupport

Hi liu,

i.MX53 supports (1866 x 1050 @60 frames per second) as

states sect.47.2.1 MX53 RM. "U:1920*1080P-56" is supported as well.

However for testing better to use OBDS, it is simpler and allows

easily to printf and modify regisers

IMX53_QSB_OBDS "On-Board Diagnostic Suit for the i.MX53 Quick Start Board"

http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=IMX53QSB&fpsp=1&tab=Design_Tools_Tab

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos

40 Views
leeo
Contributor I

hi chipexpert๏ผš

  we have requrement 1080P for  customer .

  I want to know why I can't measure the CLK of LVDS pin.

Please see attached file. Is there something wrong with sch?

0 Kudos