some questions about the use of the HAB in imx6 ROM

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

some questions about the use of the HAB in imx6 ROM

ソリューションへジャンプ
803件の閲覧回数
guokaizhao
Contributor I

(1)Whether The program in ROM which use the HAB run in trustzone.

(2)Is IMX6 on-chip ROM program fixed in factory, or we can customize it ourselves.If we can customize the programs in the ROM, can you provide the sample source code for customize.

(3)If The ROM program which use the HAB operation on-chip resources will conflict with the following initialization in uboot and Linux kernel.

ラベル(1)
0 件の賞賛
返信
1 解決策
727件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hello,

  Please look at my comments below.

 

1.
The boot ROM works in secure world.

 

2.

  The boot ROM is mask programmed and cannot be changed by customers.

 

3.

  The HAB boot is used to load U-boot, and boot ROM configuration can be
reprogrammed by U-boot.

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
728件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hello,

  Please look at my comments below.

 

1.
The boot ROM works in secure world.

 

2.

  The boot ROM is mask programmed and cannot be changed by customers.

 

3.

  The HAB boot is used to load U-boot, and boot ROM configuration can be
reprogrammed by U-boot.

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信