some problem with imx233

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

some problem with imx233

2,233 Views
chengyouping
Contributor I

download updated imx233 bsp and install ltib,

1. ltib gst-plugin have no mfw_mp3_encoder.

setup was as following:

./ltib -c

select gst-plugin,gstream -plug-base,gst-plug-good, CFimager the imx23_linux.sb and rootfs.ext.gz 's content to sd card,boot imx233 dvk,

root@freescale ~$ cd /

root@freescale /$ gst-inspect |grep mfw

mfw_mpeg4aspdecoder:  mfw_mpeg4aspdecoder: Freescale MPEG4 Decoder

mfw_v4lsink:  mfw_v4lsink: Freescale: V4L Sink

mfw_aacdecoder:  mfw_aacdecoder: Freescale AAC Decoder Plugin

mfw_mp3decoder:  mfw_mp3decoder: freescale mp3 decoder

mfw_mp4demuxer:  mfw_mp4demuxer: FSL MP4 Demuxer

mfw_avidemuxer:  mfw_avidemuxer: FSL Avi Demuxer

mfw_h264decoder:  mfw_h264decoder: Freescale    H264 decoder

root@freescale /$

//no mfw_mp3encoder: freescale mp3 encoder,can't excute mp3 encoder.

2. select

./ltib -c

select fsl-mm-codec-libs and fsl-mm-mp3enc-libs

can't get fsl-mm-mp3enc-codeclib.1.8.0.tar.gz.

3.

./ltib -c

select fsl-mm-codec-libs only.

no test_mp3_enc_arm9_elinux and lib_mp3_enc_arm9_elinux.so

can't exectue mp3 encode either..

//---------------------------------------------------------------------------------

download updated imx28 multimedai framework.

L2.6.35_1.1.0_130130_MM_CODECS_BUNDLE.tar

re-install ltib.

the result is as attachment.

all in one word,

there are some error in imx233/imx28 mp3 encoder,

could someone help me ?

Labels (1)
0 Kudos
Reply
2 Replies

1,823 Views
PeterChan
NXP Employee
NXP Employee

The codec package fsl-mm-1.80.tar.gz does not possess the mfw_mp3encoder element and thus mp3 encode is not supported.

I tried the L2.6.35_1.1.0_130130_MM_CODECS on BSP L2.6.35_1.1.0 using i.MX28 and got similar errors. It looks mp3 encode do not work in i.MX233 & i.MX28.

0 Kudos
Reply

1,823 Views
PeterChan
NXP Employee
NXP Employee

Hello Cheng youping,

FYI, the mp3 encoding issue is resolved in community and you can apply the solution at Can't encode mp3 on imx28

0 Kudos
Reply