some error occured when I "bitbake fsl-image-gui"

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

some error occured when I "bitbake fsl-image-gui"

5,019 Views
azmatliu
Contributor III
ubuntu@ubuntu-virtual-machine:~/fsl-bsp/imx6q-fb$ bitbake fsl-image-gui
NOTE: Your conf/bblayers.conf has been automatically updated.
Loading cache: 100% |###########################################| ETA:  00:00:00
Loaded 2791 entries from dependency cache.
Parsing recipes: 100% |#########################################| Time: 00:00:01
Parsing of 2215 .bb files complete (2200 cached, 15 parsed). 2790 targets, 434 skipped, 5 masked, 0 errors.
NOTE: Resolving any missing task queue dependencies
Build Configuration:
BB_VERSION        = "1.30.0"
BUILD_SYS         = "x86_64-linux"
NATIVELSBSTRING   = "Ubuntu-14.04"
TARGET_SYS        = "arm-poky-linux-gnueabi"
MACHINE           = "imx6qsabresd"
DISTRO            = "fsl-imx-fb"
DISTRO_VERSION    = "4.1.15-2.1.0"
TUNE_FEATURES     = "arm armv7a vfp  neon        callconvention-hard        cortexa9"
TARGET_FPU        = "hard"
meta             
meta-yocto        = "HEAD:f5da2a5913319ad6ac2141438ba1aa17576326ab"
meta-oe          
meta-multimedia   = "HEAD:247b1267bbe95719cd4877d2d3cfbaf2a2f4865a"
meta-fsl-arm      = "HEAD:be78894e4682f111575470fb23e51e6ba523508d"
meta-fsl-arm-extra = "HEAD:3dfb82fc7e703eae9891b3ffda0e9393701f2396"
meta-fsl-demos    = "HEAD:a165068f8a0d1cf29aabe4b4053f28be1c2aa492"
meta-bsp         
meta-sdk          = "HEAD:823b26a67261270d2bf22d511e6190641a8a90cf"
meta-browser      = "HEAD:77736988073a5d90fcff9d0005c8477332ede387"
meta-gnome       
meta-networking  
meta-python      
meta-filesystems  = "HEAD:247b1267bbe95719cd4877d2d3cfbaf2a2f4865a"
meta-qt5          = "HEAD:ccae79be69c5268df3b47e4e14cea0591c39a531"
NOTE: Preparing RunQueue
NOTE: Executing SetScene Tasks
NOTE: Executing RunQueue Tasks
ERROR: gnu-config-native-20150728+gitAUTOINC+b576fa87c1-r0 do_unpack: Function failed: Fetcher failure: Fetch command failed with exit code 128, output:
fatal: the '--set-upstream' option is no longer supported. Please use '--track' or '--set-upstream-to' instead.
ERROR: Logfile of failure stored in: /home/ubuntu/fsl-bsp/imx6q-fb/tmp/work/x86_64-linux/gnu-config-native/20150728+gitAUTOINC+b576fa87c1-r0/temp/log.do_unpack.3615
Log data follows:
| DEBUG: Executing python function do_unpack
| DEBUG: Executing python function base_do_unpack
| DEBUG: Running export DBUS_SESSION_BUS_ADDRESS="unix:abstract=/tmp/dbus-bOMf6q5O0B"; export SSH_AUTH_SOCK="/run/user/1000/keyring-vaybsv/ssh"; export PATH="/home/ubuntu/fsl-bsp/sources/poky/scripts/native-intercept:/home/ubuntu/fsl-bsp/sources/poky/scripts:/home/ubuntu/fsl-bsp/imx6q-fb/tmp/sysroots/x86_64-linux/usr/bin/x86_64-linux:/home/ubuntu/fsl-bsp/imx6q-fb/tmp/sysroots/x86_64-linux/usr/bin:/home/ubuntu/fsl-bsp/imx6q-fb/tmp/sysroots/x86_64-linux/usr/sbin:/home/ubuntu/fsl-bsp/imx6q-fb/tmp/sysroots/x86_64-linux/usr/bin:/home/ubuntu/fsl-bsp/imx6q-fb/tmp/sysroots/x86_64-linux/sbin:/home/ubuntu/fsl-bsp/imx6q-fb/tmp/sysroots/x86_64-linux/bin:/home/ubuntu/fsl-bsp/sources/poky/scripts:/home/ubuntu/fsl-bsp/sources/poky/bitbake/bin:/home/ubuntu/bin:/home/ubuntu/bin:/usr/local/sbin:/usr/local/bin:/usr/sbin:/usr/bin:/sbin:/bin:/usr/games:/usr/local/games"; export HOME="/home/ubuntu"; git -c core.fsyncobjectfiles=0 clone -s -n /home/ubuntu/fsl-bsp/downloads//git2/git.sv.gnu.org.config.git/ /home/ubuntu/fsl-bsp/imx6q-fb/tmp/work/x86_64-linux/gnu-config-native/20150728+gitAUTOINC+b576fa87c1-r0/git/
| DEBUG: Running export DBUS_SESSION_BUS_ADDRESS="unix:abstract=/tmp/dbus-bOMf6q5O0B"; export SSH_AUTH_SOCK="/run/user/1000/keyring-vaybsv/ssh"; export PATH="/home/ubuntu/fsl-bsp/sources/poky/scripts/native-intercept:/home/ubuntu/fsl-bsp/sources/poky/scripts:/home/ubuntu/fsl-bsp/imx6q-fb/tmp/sysroots/x86_64-linux/usr/bin/x86_64-linux:/home/ubuntu/fsl-bsp/imx6q-fb/tmp/sysroots/x86_64-linux/usr/bin:/home/ubuntu/fsl-bsp/imx6q-fb/tmp/sysroots/x86_64-linux/usr/sbin:/home/ubuntu/fsl-bsp/imx6q-fb/tmp/sysroots/x86_64-linux/usr/bin:/home/ubuntu/fsl-bsp/imx6q-fb/tmp/sysroots/x86_64-linux/sbin:/home/ubuntu/fsl-bsp/imx6q-fb/tmp/sysroots/x86_64-linux/bin:/home/ubuntu/fsl-bsp/sources/poky/scripts:/home/ubuntu/fsl-bsp/sources/poky/bitbake/bin:/home/ubuntu/bin:/home/ubuntu/bin:/usr/local/sbin:/usr/local/bin:/usr/sbin:/usr/bin:/sbin:/bin:/usr/games:/usr/local/games"; export HOME="/home/ubuntu"; git -c core.fsyncobjectfiles=0 remote set-url origin git://git.sv.gnu.org/config.git
| DEBUG: Running export DBUS_SESSION_BUS_ADDRESS="unix:abstract=/tmp/dbus-bOMf6q5O0B"; export SSH_AUTH_SOCK="/run/user/1000/keyring-vaybsv/ssh"; export PATH="/home/ubuntu/fsl-bsp/sources/poky/scripts/native-intercept:/home/ubuntu/fsl-bsp/sources/poky/scripts:/home/ubuntu/fsl-bsp/imx6q-fb/tmp/sysroots/x86_64-linux/usr/bin/x86_64-linux:/home/ubuntu/fsl-bsp/imx6q-fb/tmp/sysroots/x86_64-linux/usr/bin:/home/ubuntu/fsl-bsp/imx6q-fb/tmp/sysroots/x86_64-linux/usr/sbin:/home/ubuntu/fsl-bsp/imx6q-fb/tmp/sysroots/x86_64-linux/usr/bin:/home/ubuntu/fsl-bsp/imx6q-fb/tmp/sysroots/x86_64-linux/sbin:/home/ubuntu/fsl-bsp/imx6q-fb/tmp/sysroots/x86_64-linux/bin:/home/ubuntu/fsl-bsp/sources/poky/scripts:/home/ubuntu/fsl-bsp/sources/poky/bitbake/bin:/home/ubuntu/bin:/home/ubuntu/bin:/usr/local/sbin:/usr/local/bin:/usr/sbin:/usr/bin:/sbin:/bin:/usr/games:/usr/local/games"; export HOME="/home/ubuntu"; git -c core.fsyncobjectfiles=0 checkout -B master b576fa87c140b824466ef1638e945e87dc5c0343
| DEBUG: Running export DBUS_SESSION_BUS_ADDRESS="unix:abstract=/tmp/dbus-bOMf6q5O0B"; export SSH_AUTH_SOCK="/run/user/1000/keyring-vaybsv/ssh"; export PATH="/home/ubuntu/fsl-bsp/sources/poky/scripts/native-intercept:/home/ubuntu/fsl-bsp/sources/poky/scripts:/home/ubuntu/fsl-bsp/imx6q-fb/tmp/sysroots/x86_64-linux/usr/bin/x86_64-linux:/home/ubuntu/fsl-bsp/imx6q-fb/tmp/sysroots/x86_64-linux/usr/bin:/home/ubuntu/fsl-bsp/imx6q-fb/tmp/sysroots/x86_64-linux/usr/sbin:/home/ubuntu/fsl-bsp/imx6q-fb/tmp/sysroots/x86_64-linux/usr/bin:/home/ubuntu/fsl-bsp/imx6q-fb/tmp/sysroots/x86_64-linux/sbin:/home/ubuntu/fsl-bsp/imx6q-fb/tmp/sysroots/x86_64-linux/bin:/home/ubuntu/fsl-bsp/sources/poky/scripts:/home/ubuntu/fsl-bsp/sources/poky/bitbake/bin:/home/ubuntu/bin:/home/ubuntu/bin:/usr/local/sbin:/usr/local/bin:/usr/sbin:/usr/bin:/sbin:/bin:/usr/games:/usr/local/games"; export HOME="/home/ubuntu"; git -c core.fsyncobjectfiles=0 branch --set-upstream master origin/master
| DEBUG: Python function base_do_unpack finished
| DEBUG: Python function do_unpack finished
| ERROR: Function failed: Fetcher failure: Fetch command failed with exit code 128, output:
| fatal: the '--set-upstream' option is no longer supported. Please use '--track' or '--set-upstream-to' instead.
|
ERROR: Task 531 (virtual:native:/home/ubuntu/fsl-bsp/sources/poky/meta/recipes-devtools/gnu-config/gnu-config_git.bb, do_unpack) failed with exit code '1'
NOTE: Tasks Summary: Attempted 11 tasks of which 9 didn't need to be rerun and 1 failed.
Waiting for 0 running tasks to finish:
Summary: 1 task failed:
  virtual:native:/home/ubuntu/fsl-bsp/sources/poky/meta/recipes-devtools/gnu-config/gnu-config_git.bb, do_unpack
Summary: There was 1 ERROR message shown, returning a non-zero exit code.
ubuntu@ubuntu-virtual-machine:~/fsl-bsp/imx6q-fb$ ls /usr/bin/python3 -l
lrwxrwxrwx 1 root root 9 Jul 31 20:45 /usr/bin/python3 -> python3.4
please help~~  TT
Labels (3)
Tags (2)
0 Kudos
Reply
3 Replies

2,278 Views
azmatliu
Contributor III

 I found that my git version was 2.15.0(Ubuntu 14.04),then I updated git to V2.7.0.It work!

0 Kudos
Reply

2,278 Views
b36401
NXP Employee
NXP Employee

OK.
Thanx for letting us know.

Have a great day,
Victor

0 Kudos
Reply

2,278 Views
azmatliu
Contributor III

I am waiting~

0 Kudos
Reply