Hi,
I'm trying build an image yocto with gstreamer. I added on local.conf file the IMAGE_INSTALL_append: "gst-plugins-base-meta gst-plugins-good-meta gst-ffmpeg gst-fsl-plugin" modules, and executed the process from this link: https://community.freescale.com/docs/DOC-93688
The output from the command "gst-launch v4l2src ! mfw_v4lsink" is:
root@cgtqmx6:~# gst-launch v4l2src ! mfw_v4lsink
MFW_GST_V4LSINK_PLUGIN 3.0.11 build on Jul 30 2015 17:48:50.
Setting pipeline to PAUSED ...
ERROR: Pipeline doesn't want to pause.
ERROR: from element /GstPipeline:pipeline0/GstV4l2Src:v4l2src0: Cannot identify device '/dev/video0'.
Additional debug info:
/home/polosulorg/yocto/bsp-scripts/build/tmp/work/cortexa9hf-vfp-neon-poky-linux-gnueabi/gst-plugins-good/0.10.31-r8/gst-plugins-good-0.10.31/sys/v4l2/v4l2_calls.c(498): gst_v4l2_open (): /GstPipeline:pipeline0/GstV4l2Src:v4l2src0:
system error: No such file or directory
Setting pipeline to NULL ...
Total rendered:0
Freeing pipeline ...
[--->FINALIZE v4l_sink
The device is not creating the /dev/video0. To create a new /dev/video0 I'm executing the command "mknod /dev/video0 c 81 0". After it, the output from the command "gst-launch v4l2src ! mfw_v4lsink" is:
root@cgtqmx6:~# gst-launch v4l2src ! mfw_v4lsink
MFW_GST_V4LSINK_PLUGIN 3.0.11 build on Jul 30 2015 17:48:50.
Setting pipeline to PAUSED ...
ERROR: Pipeline doesn't want to pause.
ERROR: from element /GstPipeline:pipeline0/GstV4l2Src:v4l2src0: Could not open device '/dev/video0' for reading and writing.
Additional debug info:
/home/polosulorg/yocto/bsp-scripts/build/tmp/work/cortexa9hf-vfp-neon-poky-linux-gnueabi/gst-plugins-good/0.10.31-r8/gst-plugins-good-0.10.31/sys/v4l2/v4l2_calls.c(512): gst_v4l2_open (): /GstPipeline:pipeline0/GstV4l2Src:v4l2src0:
system error: No such device or address
Setting pipeline to NULL ...
Total rendered:0
Freeing pipeline ...
[--->FINALIZE v4l_sink
Can you help-me?
Thanks
已解决! 转到解答。
Problem solved. I bought a new USB Camera with another driver. It's work perfectly.
Thank you so much.
Hi Mauricio Karrei,
I am very glad you have solved your problem. So I closed this thread, if you have any other questions you can create new threads in our community.
Have a nice day.
Best Regards
Dan