setplayspeed

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
1,930件の閲覧回数
weikeng-jimmy
Contributor III

Hi Sir,

I found android API in the Android_codec_release_note as below . The "setPlaySpeed" is only for audio track ? Or it can make the video frame rewind/forward ?

Thanks!

6 Extend Android Multimedia Framework APIs
In Jelly Bean, Freescale has extended only one Android API, set playback speed.
/* trick mode */
/**
* Set playback speed.
*
* @param Speed[] contains only one item which is normalized speed multiplied by 0x10000
* Range of normalized speed is:
* [-16,-2] means rewind, [0.1, 16] means fast forward, step is 0.1
* when normalized speed is [0.1, 1.9] audio is outputted, otherwise audio
* is not outputted.
* After this function call returns, result speed is stored in Speed[0], to show whether
it succeeds or fails.
*/
public native void setPlaySpeed(int[] Speed);

ラベル(3)
0 件の賞賛
返信
1 解決策
1,616件の閲覧回数
joanxie
NXP TechSupport
NXP TechSupport

I've updated in your SR, if any update, pls let me know it, if no, pls close this thread.

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,617件の閲覧回数
joanxie
NXP TechSupport
NXP TechSupport

I've updated in your SR, if any update, pls let me know it, if no, pls close this thread.

0 件の賞賛
返信