set ethernet address on usb0

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

set ethernet address on usb0

916件の閲覧回数
patrickimmling
Contributor I

Hi All,

I have an imx51 evk board. I have the freescale android image running on it(R.10.3).

I have two DHCP networks. I have one normally connected over ethernet port of the board. The other via usb port. How do I set the MAC address in my U-boot command?

I did a normal setenv ethaddr xx.xx.xx.xx.

However both the ethernet and usb0 seem to be polling their respective dhcp servers without reply.

Can the ethaddr overwrite the previous addresS?

How can I get the two dhcp-based network interfaces runing?

Please help

タグ(2)
0 件の賞賛
返信
0 返答(返信)