sensor SC1330T porting on imx8mp

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

sensor SC1330T porting on imx8mp

1,654 Views
wangbaoC
Contributor I

Dear NXP Team,

We want to port the sensor SC1330T on imx8mp, we modified the sensor driver in ov5645, then use  cmd

"gst-launch-1.0 v4l2src device=/dev/video0 ! autovideosink" , we could get image on the screen(hdmi), but the image is not  full of it . check it below

Could you pls help us to check it?

Thanks a lot

0 Kudos
Reply
1 Reply

1,625 Views
Sanket_Parekh
NXP TechSupport
NXP TechSupport
 
I hope you are doing well
 
Are you using both CSI ports simultaneously?
Please share which modification you have done in the sensor driver for ov5645.
 
To debug the issue,
One can check the display resolution according to section 1.4.2.12 Display Interfaces from the Reference manual IMX8MPRM.
Kindly verify the parameter for MIPI Interface according to Table 1. Features from the datasheet IMX8MPIEC.
 
For the information related to the GStreamer pipeline, please refer to the below document.
 
Thanks & Regards
Sanket Parekh
0 Kudos
Reply