Hi
I am working on secure boot with sabrelite board.(Freescale i.MX6Q rev1.0 at 792 MHz)
I am using code base "uboot-imx-imx_v2013.04_3.10.17_1.0.0_beta"
I am facing hab event issue when we issue hab_status command , Please provide your inputs.
I have provided the image, signing and event detail info below.
Image Detail:-
tools/mkimage -l u-boot.imx
Image Type: Freescale IMX Boot Image
Image Ver: 2 (i.MX53/6 compatible)
Mode: DCD
Secure Boot Mode: ON
CSF Data Address: 17850000
U-Boot Data Size: 357376 Bytes = 349.00 kB = 0.34 MB
U-Boot Load Address: 177fac00
U-Boot Entry Point: 17800000
signing Detail:-
we are using following referance link sign the image.
“https://community.freescale.com/docs/DOC-96451"
csf_u-boot_yocto.txt file:-
[Header]
Version = 4.1
Hash Algorithm = sha256
Engine Configuration = 0
Certificate Format = X509
Signature Format = CMS
[Install SRK]
File = "../crts/SRK_1_2_3_4_table.bin"
Source index = 0
[Install CSFK]
File = "../crts/CSF1_1_sha256_4096_65537_v3_usr_crt.pem"
[Authenticate CSF]
[Unlock]
Engine = CAAM
Features = RNG
[Install Key]
Verification index = 0
Target index = 2
File = "../crts/IMG1_1_sha256_4096_65537_v3_usr_crt.pem"
# Sign padded u-boot starting at the IVT through to the end with
# length = 0x5D000 (padded u-boot length)
# This covers the essential parts: IVT, boot data and DCD.
# Blocks have the following definition:
# Image block start address on i.MX, Offset from start of image file,
# Length of block in bytes, image data file
[Authenticate Data]
Verification index = 2
Blocks = 0x177FB000 0x0 0x55000 "u-boot-pad.bin"
Command :-
/opt/tooling/codesourcery/MGC-2013.11-73-gcc-4.8.1/Sourcery_CodeBench_for_ARM_GNU_Linux/bin/arm-none-linux-gnueabi-objcopy -I binary -O binary --pad-to 0x55000 --gap-fill=0xff u-boot.imx u-boot-pad.bin
../linux/cst --output csf_u-boot.bin < csf_u-boot_yocto.txt
cat u-boot-pad.bin csf_u-boot.bin > u-boot-signed.bin
Event Detail:-
If we issue hab_status command we are getting following events:-
MX6QSABRELITE U-Boot > hab_status
iMX6 HAB status Information :
=============================
HAB Configuration: 0xf0, HAB State: 0x66
--------- HAB Event 1 -----------------
event data:
0xdb 0x00 0x14 0x41 0x33 0x0c 0xa0 0x00
0x00 0x00 0x00 0x00 0x17 0x7f 0xb0 0x00
0x00 0x00 0x00 0x20
--------- HAB Event 2 -----------------
event data:
0xdb 0x00 0x14 0x41 0x33 0x0c 0xa0 0x00
0x00 0x00 0x00 0x00 0x17 0x7f 0xb0 0x2c
0x00 0x00 0x02 0xf0
--------- HAB Event 3 -----------------
event data:
0xdb 0x00 0x14 0x41 0x33 0x0c 0xa0 0x00
0x00 0x00 0x00 0x00 0x17 0x7f 0xb0 0x20
0x00 0x00 0x00 0x01
--------- HAB Event 4 -----------------
event data:
0xdb 0x00 0x14 0x41 0x33 0x0c 0xa0 0x00
0x00 0x00 0x00 0x00 0x17 0x80 0x00 0x00
0x00 0x00 0x00 0x04
--------- HAB Event 5 -----------------
event data:
0xdb 0x00 0x14 0x41 0x33 0x21 0xc0 0x00
0xbe 0x00 0x0c 0x00 0x03 0x17 0x00 0x00
0x00 0x00 0x00 0x50
Hi Ajay,
Your log indicates that your certificate is invalid:
------------+----+------+----+-------------------------------------------------
Event |0xdb|0x0014|0x41| SRCE Field: 33 21 c0 00
| | | | STS = HAB_FAILURE (0x33)
| | | | RSN = HAB_INV_CERTIFICATE (0x21)
| | | | CTX = HAB_CTX_COMMAND (0xC0)
| | | | ENG = HAB_ENG_ANY (0x00)
| | | | Cmd Field: 0xbe000c00
| | | | CMD: HAB_CMD_INS_KEY (0xbe)
| | | | LEN: 0x000c
| | | | FLG: 0x03
| | | | FLAGS: NOTHING YET
| | | | PAST Field: 0x03170000
| | | | Crt. addr: 0x00000050
------------+----+------+----+-------------------------------------------------
Since you are doing normal secure boot, your SRK need to have th CA flag set. In the questions made by the hab4_pki_tree, you need to answer : 'n',4096,'10',4,'y'.
If the last anser is 'n', then the pki will be generated for fast authentication.
You can check this using:
openssl x509 -in SRK1_sha256_4096_65537_v3_ca_crt.pem -text -noout | less
Then look for CA: True.
if its false then you will need to change your CSF to:
[Header]
Version = 4.1
[Install SRK]
File = "../crts/SRK_1_2_3_4_table.bin"
Source index = 0
[Install NOCAK]
File = "../crts/SRK1_sha256_4096_65537_v3_usr_crt.pem"
[Authenticate CSF]
[Authenticate Data]
Verification index = 0
Blocks = %load_addr% 0x00000000 %ivt_dcd_size% "u-boot.imx"
Also, it looks that your blocks are a little bit off.
"Blocks = 0x177FB000 0x0 0x55000 "u-boot-pad.bin""
I believe the first block is wrong, this should be the address of the IVT, which looks to me that it might be at 177FA000.
Regards,
Ulises
Hi Ulises,
Thanks for reply.
I have checked openssl x509 -in SRK1_sha256_4096_65537_v3_ca_crt.pem -text -noout | less . Its value is "true"
I believe the first block is correct only.
$ od -x -N 64 u-boot-signed.bin
0000000 00d1 4020 0000 1780 0000 0000 b02c 177f
0000020 b020 177f b000 177f 0000 1785 0000 0000
0000040 ac00 177f 7400 0005 0000 0000 02d2 40f0
0000060 02cc 04ec 0e02 9807 0c00 0000 0e02 5807
0000100
IVT.Self is 0x177fb000.
Best Regards
Ajay
Hi Ajay
i.MX6Q rev1.0 (preproduction parts) were not tested with
BSPs and may not work properly, refer to part of Release Notes
also on these parts OTPMK are not burned, from attached
i.MX_6_Linux_High_Assurance_Boot_(HAB)_User's_Guide.pdf
In general recommended to use latest GA release, not beta
L3.14.28_1.0.0_iMX6QDLS_BUNDLE
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Igor,
Thank you for Reply.
I have flashed OTPMK register, Still I am getting same events.
I have checked SNVS_HP Status Register, but I am not bale to interpret is it correct or some thing is wrong?
SNVS_HP Status Register log:-
MX6QSABRELITE U-Boot > md.l 0x20CC014
020cc014: 80000b00 00000000 00000000 00000000 ................
020cc024: 00000000 00000000 00000000 00000000 ................
020cc034: 00000000 00000000 00000000 00000000 ................
020cc044: 00000000 00000000 00000008 00000000 ................
020cc054: 00000000 00000000 00000000 00000000 ................
020cc064: 00000000 00000000 00000000 00000000 ................
Please find OTPMK flash success log:-
MX6Q SABRELITE U-Boot > imxotp blow --force 0x10 0x975b69a7
Current fuse at (index: 0x10) value: 0x0
Blowing fuse at index: 0x10, value: 0x975B69A7
Reloading shadow registers...
Operation succeeded fuse at (index: 0x10) value: 0x975B69A7
MX6Q SABRELITE U-Boot > imxotp blow --force 0x11 0xafae0b5d
Current fuse at (index: 0x11) value: 0x0
Blowing fuse at index: 0x11, value: 0xAFAE0B5D
Reloading shadow registers...
Operation succeeded fuse at (index: 0x11) value: 0xAFAE0B5D
MX6Q SABRELITE U-Boot > imxotp blow --force 0x12 0x6f780499
Current fuse at (index: 0x12) value: 0x0
Blowing fuse at index: 0x12, value: 0x6F780499
Reloading shadow registers...
Operation succeeded fuse at (index: 0x12) value: 0x6F780499
MX6Q SABRELITE U-Boot > imxotp blow --force 0x13 0x3dda7a47
Current fuse at (index: 0x13) value: 0x0
Blowing fuse at index: 0x13, value: 0x3DDA7A47
Reloading shadow registers...
Operation succeeded fuse at (index: 0x13) value: 0x3DDA7A47
MX6Q SABRELITE U-Boot > imxotp blow --force 0x14 0x76fcba3c
Current fuse at (index: 0x14) value: 0x0
Blowing fuse at index: 0x14, value: 0x76FCBA3C
Reloading shadow registers...
Operation succeeded fuse at (index: 0x14) value: 0x76FCBA3C
MX6Q SABRELITE U-Boot > imxotp blow --force 0x15 0x6d5c9ef6
Current fuse at (index: 0x15) value: 0x0
Blowing fuse at index: 0x15, value: 0x6D5C9EF6
Reloading shadow registers...
Operation succeeded fuse at (index: 0x15) value: 0x6D5C9EF6
MX6Q SABRELITE U-Boot > imxotp blow --force 0x16 0xb166b40a
Current fuse at (index: 0x16) value: 0x0
Blowing fuse at index: 0x16, value: 0xB166B40A
Reloading shadow registers...
Operation succeeded fuse at (index: 0x16) value: 0xB166B40A
MX6Q SABRELITE U-Boot > imxotp blow --force 0x17 0x8f449c5d
Current fuse at (index: 0x17) value: 0x0
Blowing fuse at index: 0x17, value: 0x8F449C5D
Reloading shadow registers...
Operation succeeded fuse at (index: 0x17) value: 0x8F449C5D
SNVS_HP Detail:-
Best Regards
Ajay