secure boot on imx6q

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

secure boot on imx6q

跳至解决方案
2,530 次查看
brian_kim
Contributor II

I am trying to finalize setting up secure boot on our custom board with i.MX6.

Now, hab_status returned events (failure) but I don't know why it returned failure message.

This is sequnce and log about my work.

1)

./hab4_pki_tree.sh

Do you want to use an existing CA key (y/n)?: n

Do you want to use Elliptic Curve Cryptography (y/n)?: n

Enter key length in bits for PKI tree: 2048

Enter PKI tree duration (years): 10

How many Super Root Keys should be generated? 4

Do you want the SRK certificates to have the CA flag set? (y/n)?: y

2)

./srktool -h 4 -t SRK_1_2_3_4_table.bin -e SRK_1_2_3_4_fuse.bin -d sha256 -c \

./SRK1_sha256_2048_65537_v3_ca_crt.pem,./SRK2_sha256_2048_65537_v3_ca_crt.pem,\

./SRK3_sha256_2048_65537_v3_ca_crt.pem,./SRK4_sha256_2048_65537_v3_ca_crt.pem -f 1

3)

hexdump -e '/4 "0x"' -e '/4 "%X""\n"' SRK_1_2_3_4_fuse.bin

get 8 keys

4) in uboot prompt

fuse prog 3 0 key00

~

fuse prog 3 7 key07

5) add CONFIG_SECURE_BOOT

imx6q_uboot/include/configs$ vi xxx_config.h

/* uncomment for SECURE mode support */

#define CONFIG_SECURE_BOOT

#ifdef CONFIG_SECURE_BOOT

#ifndef CONFIG_CSF_SIZE

#define CONFIG_CSF_SIZE 0x4000

#endif

#endif

6) make u-boot.imx

dd if=./u-boot.imx bs=4 count=12 2>/dev/null | hexdump -v -e '/4 "%04_ax: "' -e '/4 "%08X" "\n"'

0000: 402000D1

0004: 17800000

0008: 00000000

000c: 177FF42C

0010: 177FF420

0014: 177FF400

0018: 00000000

001c: 00000000

0020: 177FF000

0024: 00070000

0028: 00000000

002c: 401803D2

7)

cat csf-uboot

=====================================================

#Illustrative Command Sequence File Description

[Header]

Version = 4.1

Hash Algorithm = sha256

Engine = ANY

Engine Configuration = 0

Certificate Format = X509

Signature Format = CMS

[Install SRK]

File = "../crts/SRK_1_2_3_4_table.bin"

Source index = 0 # Index of the key location in the SRK table to be installed

[Install CSFK]

# Key used to authenticate the CSF data

File = "../crts/CSF1_1_sha256_2048_65537_v3_usr_crt.pem"

[Authenticate CSF]

[Unlock]

Engine = CAAM

Features = RNG

[Install Key]

# Key slot index used to authenticate the key to be installed

Verification index = 0

# Target key slot in HAB key store where key will be installed

Target Index = 2

# Key to install

File= "../crts/IMG1_1_sha256_2048_65537_v3_usr_crt.pem"

[Authenticate Data]

# Key slot index used to authenticate the image data

Verification index = 2

# Address Offset Length Data File Path

Blocks = 0x177FF400 0x000 0x6fc00 "./bin/u-boot.imx"

======================================================

0x6fc00 is size of u-boot.imx

8)

./cst -o csf-uboot.bin -i csf-uboot

9)

cat ./bin/u-boot.imx csf-uboot.bin > u-boot-signed.imx

10)

=> hab_status

Secure boot disabled

HAB Configuration: 0xf0, HAB State: 0x66

--------- HAB Event 1 -----------------

event data:

        0xdb 0x00 0x08 0x41 0x33 0x22 0x0a 0x00

--------- HAB Event 2 -----------------

event data:

        0xdb 0x00 0x14 0x41 0x33 0x0c 0xa0 0x00

        0x00 0x00 0x00 0x00 0x17 0x7f 0xf4 0x00

        0x00 0x00 0x00 0x20

--------- HAB Event 3 -----------------

event data:

        0xdb 0x00 0x14 0x41 0x33 0x0c 0xa0 0x00

        0x00 0x00 0x00 0x00 0x17 0x7f 0xf4 0x2c

        0x00 0x00 0x03 0x18

--------- HAB Event 4 -----------------

event data:

        0xdb 0x00 0x14 0x41 0x33 0x0c 0xa0 0x00

        0x00 0x00 0x00 0x00 0x17 0x7f 0xf4 0x20

        0x00 0x00 0x00 0x01

--------- HAB Event 5 -----------------

event data:

        0xdb 0x00 0x14 0x41 0x33 0x0c 0xa0 0x00

        0x00 0x00 0x00 0x00 0x17 0x80 0x00 0x00

        0x00 0x00 0x00 0x04

What is the reason of issue ?

标签 (2)
0 项奖励
回复
1 解答
1,802 次查看
brian_kim
Contributor II
0 项奖励
回复
2 回复数
1,803 次查看
brian_kim
Contributor II

I was solved problem with below URL.

Encrypted boot loader on SabreSD i.MX6q board

0 项奖励
回复
1,802 次查看
kinezo
Contributor III

Hey brian.kim‌, what part of the solution in that URL helped you fix your problem? I'm having the exact same HAB Events as you showed above, and I can't find a definitive answer as to how to fix this "HAB_INV_ADDRESS" (0x22) error.

0 项奖励
回复