secure boot on an imx7dsabre

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

secure boot on an imx7dsabre

1,032 次查看
nahomab
Contributor I

Hi

I am trying to implement secure boot on an imx7dsabre and I am having a little trouble. I looked at the other posts on the forum and still couldn't resolve the issues.

Here is what I did:

- Built u-boot from this repository: https://github.com/u-boot/u-boot

I made sure the mx7dsabresd_defconfig file included CONFIG_IMX_HAB=y and built my u-boot.imx

- Generated a PKI using cst-3.3.1

I generated 4 keys of length 4096 as well as the two files fuse.bin and table.bin. But then I only fused values of the first key onto the board, wanted to make sure everything was working fine before fusing everything else.

- Generate csf file: I generated the csf file as follows:

[Header]
Version = 4.2
Hash Algorithm = sha256
Engine = CAAM
Engine Configuration = 0
Certificate Format = X509
Signature Format = CMS

[Install SRK]
File = "../../crts/SRK_1_2_3_4_table.bin"
Source index = 0

[Install CSFK]
File = "../../crts/CSF1_1_sha256_4096_65537_v3_usr_crt.pem"

[Authenticate CSF]

[Install Key]
Verification index = 0
Target index = 2
File = "../../crts/IMG1_1_sha256_4096_65537_v3_usr_crt.pem"

[Unlock]
Engine = CAAM
Features = RNG

[Authenticate Data]
Verification index = 2
Blocks = 0x877ff400 0x00000000 0x00078c00 "u-boot.imx"

[Authenticate Data]
Verification index = 2
Blocks = 0x00910000 0x0000002c 0x000001b4 "u-boot.imx"


The log file u-boot-dtb.imb looks like this:

Image Type: Freescale IMX Boot Image
Image Ver: 2 (i.MX53/6/7 compatible)
Mode: DCD
Data Size: 503904 Bytes = 492.09 KiB = 0.48 MiB
Load Address: 877ff420
Entry Point: 87800000
HAB Blocks: 0x877ff400 0x00000000 0x00078c00
DCD Blocks: 0x00910000 0x0000002c 0x000001b4

- Signing the image: since I'll be using imx_usb to load the image onto the board, I made sure to clear the DCD table during the signing process using mod_4_mfgtool:

cst-3.3.1/linux64/bin$ ./mod_4_mfgtool.sh clear_dcd_addr u-boot.imx
cst-3.3.1/linux64/bin$ ./cst -i uboot.csf -o uboot_csf.bin
cst-3.3.1/linux64/bin$ ./mod_4_mfgtool.sh set_dcd_addr u-boot.imx
cst-3.3.1/linux64/bin$ cat u-boot.imx uboot_csf.bin > signed_u-boot

After loading the image, I get the following hab events:

=> hab_status

Secure boot disabled

HAB Configuration: 0xf0, HAB State: 0x66

--------- HAB Event 1 -----------------
event data:
0xdb 0x00 0x14 0x42 0x33 0x0c 0xa0 0x00
0x00 0x00 0x00 0x00 0x87 0x7f 0xf4 0x00
0x00 0x00 0x00 0x20

STS = HAB_FAILURE (0x33)
RSN = HAB_INV_ASSERTION (0x0C)
CTX = HAB_CTX_ASSERT (0xA0)
ENG = HAB_ENG_ANY (0x00)


--------- HAB Event 2 -----------------
event data:
0xdb 0x00 0x14 0x42 0x33 0x0c 0xa0 0x00
0x00 0x00 0x00 0x00 0x87 0x7f 0xf4 0x20
0x00 0x00 0x00 0x01

STS = HAB_FAILURE (0x33)
RSN = HAB_INV_ASSERTION (0x0C)
CTX = HAB_CTX_ASSERT (0xA0)
ENG = HAB_ENG_ANY (0x00)


--------- HAB Event 3 -----------------
event data:
0xdb 0x00 0x14 0x42 0x33 0x0c 0xa0 0x00
0x00 0x00 0x00 0x00 0x87 0x80 0x00 0x00
0x00 0x00 0x00 0x04

STS = HAB_FAILURE (0x33)
RSN = HAB_INV_ASSERTION (0x0C)
CTX = HAB_CTX_ASSERT (0xA0)
ENG = HAB_ENG_ANY (0x00)


--------- HAB Event 4 -----------------
event data:
0xdb 0x00 0x14 0x42 0x33 0x0c 0xa0 0x00
0x00 0x00 0x00 0x00 0x00 0x91 0x00 0x00
0x00 0x00 0x01 0xb4

STS = HAB_FAILURE (0x33)
RSN = HAB_INV_ASSERTION (0x0C)
CTX = HAB_CTX_ASSERT (0xA0)
ENG = HAB_ENG_ANY (0x00)


--------- HAB Event 5 -----------------
event data:
0xdb 0x00 0x14 0x42 0x33 0x21 0xc0 0x00
0xbe 0x00 0x0c 0x00 0x03 0x17 0x00 0x00
0x00 0x00 0x00 0x64

STS = HAB_FAILURE (0x33)
RSN = HAB_INV_CERTIFICATE (0x21)
CTX = HAB_CTX_COMMAND (0xC0)
ENG = HAB_ENG_ANY (0x00)

Thank you for your help.

标签 (1)
标记 (1)
0 项奖励
回复
1 回复

1,015 次查看
Zhiming_Liu
NXP TechSupport
NXP TechSupport
0 项奖励
回复