secondary QSPI boot

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

secondary QSPI boot

Jump to solution
2,241 Views
sapirbuz
Contributor IV

Hi,

We are using evaluation board IMXRT1050-EVKB and trying to boot from the secondary FlexSPI pins: 

GPIO_AD_B1_08
GPIO_AD_B1_09
GPIO_AD_B1_10
GPIO_AD_B1_11
GPIO_AD_B1_12
GPIO_AD_B1_13
GPIO_AD_B1_14
GPIO_AD_B1_15

We soldered a Flash to those pins:

sapirbuz_0-1658649995694.png

 

Our board's configuration:

BOOT_MODE[1:0]= 10 (internal boot)

BOOT_CGG[10:8]= 111

sapirbuz_1-1658650027742.png

Why does the internal boot still occur from Flash U33 (primary pins) and not from the secondary pins?

Should we do something else besides the HW setup I have mentioned?

0 Kudos
Reply
1 Solution
2,212 Views
kerryzhou
NXP TechSupport
NXP TechSupport

Hi @sapirbuz ,

   As your connection is still the flexspi 1 A port, just the secondary pinout option for FlexSPI serial NOR flash boot.

  So the address still the same from 0X60000000.

 

Wish it helps you!

Best Regards,

Kerry

View solution in original post

0 Kudos
Reply
4 Replies
2,223 Views
jay_heng
NXP Employee
NXP Employee

Your HW settings are correct for you case.

Please try to dump below registers by Jlink-Commander to double check your HW settings

SRC_SBMR1 - 0x400F8004

SRC_SBMR2 - 0x400F801C

2,217 Views
sapirbuz
Contributor IV

Our flash is IS25LP080D-JNLE-TR

datasheet: 

https://eu.mouser.com/datasheet/2/198/issi_s_a0003474186_1-2271392.pdf 

For now, we have 2 flashes connected to our board: U33 and our external flash (IS25LP080D-JNLE-TR).

For U33, the flash base address is defined as the following:

#define NOR_FLASH_START_ADDRESS (20U * 0x1000U) 

What is the base address of the secondary pins flash?

How can we program our external flash?

0 Kudos
Reply
2,213 Views
kerryzhou
NXP TechSupport
NXP TechSupport

Hi @sapirbuz ,

   As your connection is still the flexspi 1 A port, just the secondary pinout option for FlexSPI serial NOR flash boot.

  So the address still the same from 0X60000000.

 

Wish it helps you!

Best Regards,

Kerry

0 Kudos
Reply
2,179 Views
sapirbuz
Contributor IV

Thank you

0 Kudos
Reply