I have recently downloaded imx-test-3.0.35-4.0.0.tar.gz from Index of /buildsources/i/imx-test,
my kernel is 3.0.35-05524-g8513494-dirty from Android 13.4.1 for imx6.
I build the mxc_sdma_memcopy_test.c as a kernel modules and mxc_sdma_test.c as an app,
However when i run the mxc_sdma_test, i got error like this:
Unable to handle kernel NULL pointer dereference at virtual address 00000010
pgd = d2370000
[00000010] *pgd=26163831, *pte=00000000, *ppte=00000000
Internal error: Oops: 17 [#1] PREEMPT SMP
Modules linked in: sdma_test
CPU: 0 Not tainted (3.0.35-05524-g8513494-dirty #4)
PC is at sdma_write+0x27c/0x2e0 [sdma_test]
LR is at sdma_write+0x278/0x2e0 [sdma_test]
pc : [<bf00035c>] lr : [<bf000358>] psr: 60000013
sp : d236ff20 ip : c0267240 fp : 00000000
r10: 00000000 r9 : d236e000 r8 : 00000000
r7 : c07f4ce0 r6 : bf000b68 r5 : 00000000 r4 : 00000400
r3 : 00000000 r2 : 00000003 r1 : bf0003c0 r0 : 00000000
Flags: nZCv IRQs on FIQs on Mode SVC_32 ISA ARM Segment user
Control: 10c53c7d Table: 2237004a DAC: 00000015
SP: 0xd236fea0:
fea0 00000000 c004ead4 00100100 00200200 c06cf710 00000c00 2234ec00 2234f000
fec0 0000040f 00000007 bf000b68 c07f4ce0 00000000 c0044b50 00000000 bf0003c0
fee0 00000003 00000000 00000400 00000000 bf000b68 c07f4ce0 00000000 d236e000
ff00 00000000 00000000 c0267240 d236ff20 bf000358 bf00035c 60000013 ffffffff
ff20 00000000 00000000 00000001 00000000 00000000 00040028 00000003 00000002
ff40 00000000 d2322ea0 00000000 d2322ea0 00000000 be99fcbc d236ff88 c00fdc04
ff60 d2322ea0 d235a000 00000000 00000000 d2322ea0 be99fcbc 00000000 c00fde8c
ff80 00000026 00000000 00000000 00000000 00000000 be99fd18 00008411 00000004
IP: 0xc02671c0:
71c0 e517203c e59d101c e5070044 e2870030 e79a3003 e7832201 eaffffed e3a00000
71e0 eaffffeb e59a0000 e59d201c e58d3000 e59f1040 e59d3014 eb0067c5 eaffffe7
7200 e59a0000 e59d201c e58d3000 e1a03008 e59f1024 eb0067be eaffffe0 c06cf730
7220 c06b5a68 c05986a0 c06cf7d8 c06b6cbc c06cf728 c06cf740 c06cf764 c06cf7a0
7240 e92d4ff0 e1a05001 e5901050 e24dd014 e1a04000 e1a08002 e1a07003 e2406078
7260 e3510001 e510a078 e5109074 0a00002a e3a03001 e3a02002 e5803050 e1a03008
7280 e5002028 e59f2210 e59a1000 e59f020c e58d9000 eb0067f7 e5047070 e1a00006
72a0 ebfffee1 e2503000 1a00006e e3001155 e1580001 8a000065 e3580000 e5843054
R7: 0xc07f4c60:
4c60 c07f1660 c07f1660 c10d90a0 bfe07000 c07f1de0 c07f1de0 c10d6780 bfe06000
4c80 c07f2480 c07f2480 c10d6dc0 bfe05000 c07f2200 c07f2200 c10d6a00 bfe04000
4ca0 c07f1d20 c07f1d20 c10d6020 bfe03000 c07f1720 c07f1720 c10d67a0 bfe02000
4cc0 c07f2100 c07f2100 c10d6000 bfe01000 c07f1ac0 c07f1ac0 00000000 00000000
4ce0 c0916000 00000000 00000000 00000000 d9000000 00032400 00040000 00000000
4d00 00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000
4d20 00000000 00000000 000000ab 00000000 c07adb00 c0789930 c0041030 00000000
4d40 d6000ea0 d6000f00 00000000 00000000 00000000 d6298aa0 d2338b2c bf000000
R9: 0xd236df80:
df80 00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000
dfa0 00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000
dfc0 00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000
dfe0 00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000
e000 00000000 00000002 00000000 d67ba060 c07a5520 00000000 00000015 c11200e0
e020 d236e000 c003e0e0 d67ba060 d6c73ba0 00000000 c07911a0 d236fe54 d236fdb0
e040 c0570eac 00000000 00000000 00000000 00000000 00000000 01000000 00000000
e060 40028820 00000000 00000000 00000000 00000000 00000000 00000000 00000000
Process test (pid: 1393, stack limit = 0xd236e2f0)
Stack: (0xd236ff20 to 0xd2370000)
ff20: 00000000 00000000 00000001 00000000 00000000 00040028 00000003 00000002
ff40: 00000000 d2322ea0 00000000 d2322ea0 00000000 be99fcbc d236ff88 c00fdc04
ff60: d2322ea0 d235a000 00000000 00000000 d2322ea0 be99fcbc 00000000 c00fde8c
ff80: 00000026 00000000 00000000 00000000 00000000 be99fd18 00008411 00000004
ffa0: c0045304 c0045180 00000000 be99fd18 00000003 be99fcbc 00000000 be99fcbc
ffc0: 00000000 be99fd18 00008411 00000004 00000000 00000000 400ca000 00000000
ffe0: 00000000 be99fcb4 00008525 4017425c 40000010 00000003 28e04021 28ad0401
[<bf00035c>] (sdma_write+0x27c/0x2e0 [sdma_test]) from [<c00fdc04>] (vfs_write+0x9c/0x140)
[<c00fdc04>] (vfs_write+0x9c/0x140) from [<c00fde8c>] (sys_write+0x38/0x70)
[<c00fde8c>] (sys_write+0x38/0x70) from [<c0045180>] (ret_fast_syscall+0x0/0x30)
Code: e58d5000 e59cc054 e12fff3c e59f1058 (e5902010)
---[ end trace 2d5f4b7560270f24 ]---
Segmentation fault
After i learn the source code and imx-sdma.c from kernel, it looks like
when dma_channel.peripheral_type is set to IMX_DMATYPE_MEMORY,
the filed sdmac->word_size is left unconfiged(default zero) so sdma_prep_slave_sg return NULL
Is there anyone who has met this problem or anyother examples on using of dmaengine(sdma)?
Original Attachment has been moved to: imx-sdma.c.zip
Original Attachment has been moved to: mxc_sdma_memcopy_test.c.zip
Original Attachment has been moved to: mxc_sdma_test.c.zip