sdk(imx-fsl-4.14.98-2.0.0_ga) build error

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

sdk(imx-fsl-4.14.98-2.0.0_ga) build error

807 Views
allen_huang1
Contributor I

We failed to build SDK(imx-fsl-4.14.98-2.0.0_ga). Please help to give me some advice.

/home/lmy/imx-fsl/imx-fsl-4.14.98-2.0.0_ga/build-imx6dl-fb/tmp/work/cortexa9hf-neon-poky-linux-gnueabi/glibc/2.27-r0/recipe-sysroot-native/usr/bin/arm-poky-linux-gnueabi.gcc-cross-initial-arm/../../libexec/arm-poky-linux-gnueabi.gcc-cross-initial-arm/gcc/arm-poky-linux-gnueabi/7.3.0/ld:/home/lmy/imx-fsl/imx-fsl-4.14.98-2.0.0_ga/build-imx6dl-fb/tmp/work/cortexa9hf-neon-poky-linux-gnueabi/glibc/2.27-r0/build-arm-poky-linux-gnueabi/shlib.lds:155: syntax error

collect2: error: ld returned 1 exit status

make[2]: *** [/home/lmy/imx-fsl/imx-fsl-4.14.98-2.0.0_ga/build-imx6dl-fb/tmp/work/cortexa9hf-neon-poky-linux-gnueabi/glibc/2.27-r0/build-arm-poky-linux-gnueabi/libc.so] Error 1

 

Host version: ubuntu18.04LTS 64bit。

build option:DISTRO=fsl-imx-fb MACHINE=imx6dlsabresd source fsl-setup-release.sh -b build-imx6dl-fb

We modified build-imx6dl-fb/conf/local.conf and adding qtwebengine to support :IMAGE_INSTALL_append = "packagegroup-qt5-webengine"

build command:bitbake fsl-image-qt5-validation-imx

0 Kudos
Reply
1 Reply

736 Views
Yuri
NXP Employee
NXP Employee

Hello,

 

   try first to build minimal system.

 

Have a great day,

Yuri.

 

-------------------------------------------------------------------------------

Note:

- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored

 

Please open a new thread and refer to the closed one, if you have a related question at a later point in time.

0 Kudos
Reply