schematics review

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

schematics review

606 Views
shivakumar1
Contributor II

Hi 

We are using imx6ul in one of our application while referring to EVK we saw some circuits in Imx6UL EVK. same attached for your reference. we don't have any battery in our project. No need of sleep mode, deep sleep etc.

I have following queries onEVK  design.

1. PMIC_STBY_REQ what is the need of this signal. is it mandatory to use?

2.PMIC_ON_REQ what is the need of this signal. is it mandatary to use?

3. GPIO_DVFS what is the need of this signal.Is it Mandatory to use?

4. can't we give fixed nominal 1.275V to VDD_ARM_SOC_IN?

Regards

shivakumar L V

0 Kudos
1 Reply

600 Views
Yuri
NXP Employee
NXP Employee

@shivakumar1 
Hello,

  The circuits, You mentioned, are intended for quick discharging during
sequence power off -> on. This allows to avoid power up sequence violations.
Also, from i.MX 6UltraLite EVK Board Hardware User’s Guide (Rev. 1, 03/2016):
"It is important that system reset should be power down and then power on, which
will avoid boot failure caused by DVFS or DRAM (LPDDR2 if used)".

So, the design solutions of the EVK may be highly recommended. 

Regards,
Yuri.

0 Kudos