sata commands in uboot in 12.09.01.01 ltib

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

sata commands in uboot in 12.09.01.01 ltib

Jump to solution
5,144 Views
frankmiller
Contributor IV

Greetings,

We have a custom board that is based on the Sabre SDB.  We are building uboot and a kernel using the 12.09.01.01 ltib and its all booting up fine.  However, our uboot image does not seem to have the 'sata' commands enabled.  How would we go about enabling them or switching our uboot to the mainline tree to get  those commands?

Thanks,

FM

0 Kudos
Reply
1 Solution
2,132 Views
lily_zhang
NXP Employee
NXP Employee

Please enable SATA command option into U-Boot. Meanwhile, you can change configuraiton and store the boot command into SATA.  Take MX6Q SabreSD board as the example, the following changes are needed.

diff --git a/include/configs/mx6q_sabresd.h b/include/configs/mx6q_sabresd.h

index 0cd57d9..68e7bec 100644

--- a/include/configs/mx6q_sabresd.h

+++ b/include/configs/mx6q_sabresd.h

@@ -103,7 +103,7 @@

#define CONFIG_CMD_CLOCK

#define CONFIG_REF_CLK_FREQ CONFIG_MX6_HCLK_FREQ

-/* #define CONFIG_CMD_SATA */

+#define CONFIG_CMD_SATA

#undef CONFIG_CMD_IMLS

#define CONFIG_CMD_IMX_DOWNLOAD_MODE

@@ -300,9 +300,9 @@

#define CONFIG_SYS_NO_FLASH

/* Monitor at beginning of flash */

-#define CONFIG_FSL_ENV_IN_MMC

+/* #define CONFIG_FSL_ENV_IN_MMC */

/* #define CONFIG_FSL_ENV_IN_NAND */

-/* #define CONFIG_FSL_ENV_IN_SATA */

+#define CONFIG_FSL_ENV_IN_SATA

#define CONFIG_ENV_SECT_SIZE    (8 * 1024)

#define CONFIG_ENV_SIZE CONFIG_ENV_SECT_SIZE

Lily

View solution in original post

0 Kudos
Reply
3 Replies
2,133 Views
lily_zhang
NXP Employee
NXP Employee

Please enable SATA command option into U-Boot. Meanwhile, you can change configuraiton and store the boot command into SATA.  Take MX6Q SabreSD board as the example, the following changes are needed.

diff --git a/include/configs/mx6q_sabresd.h b/include/configs/mx6q_sabresd.h

index 0cd57d9..68e7bec 100644

--- a/include/configs/mx6q_sabresd.h

+++ b/include/configs/mx6q_sabresd.h

@@ -103,7 +103,7 @@

#define CONFIG_CMD_CLOCK

#define CONFIG_REF_CLK_FREQ CONFIG_MX6_HCLK_FREQ

-/* #define CONFIG_CMD_SATA */

+#define CONFIG_CMD_SATA

#undef CONFIG_CMD_IMLS

#define CONFIG_CMD_IMX_DOWNLOAD_MODE

@@ -300,9 +300,9 @@

#define CONFIG_SYS_NO_FLASH

/* Monitor at beginning of flash */

-#define CONFIG_FSL_ENV_IN_MMC

+/* #define CONFIG_FSL_ENV_IN_MMC */

/* #define CONFIG_FSL_ENV_IN_NAND */

-/* #define CONFIG_FSL_ENV_IN_SATA */

+#define CONFIG_FSL_ENV_IN_SATA

#define CONFIG_ENV_SECT_SIZE    (8 * 1024)

#define CONFIG_ENV_SIZE CONFIG_ENV_SECT_SIZE

Lily

0 Kudos
Reply
2,132 Views
frankmiller
Contributor IV

Many thanks, this works fine!

FM

0 Kudos
Reply
2,132 Views
tonyzheng
NXP Employee
NXP Employee

learn a lot!

0 Kudos
Reply