same RAM part number but different SOM Part numbers

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

same RAM part number but different SOM Part numbers

3,028 Views
shamiullah
Contributor III

Hi everyone,

I am using MIMX8MM5DVTLZDA for NXP EVK IMX8MM and MIMX8MM3DVTLZAA for customized board.  we are using same part number RAM [MT53D512M32D2DS-053 WT:D] for both the above mentioned boards. we used the same DCD table in uboot for both the boards. But we are facing errors. Customized board is not completely booting . It is stopping middle of kernel . Please let us know for any modifications.

Please find the attached text file for logs

Thanks & Regards

Shamiullah

0 Kudos
Reply
2 Replies

3,023 Views
igorpadykov
NXP Employee
NXP Employee

Hi Shamiullah

 

for that issue may be recommended to run ddr test (use latest RPA tool) and rebuild image as

described in  MSCALE_DDR_Tool_User_Guide.pdf

https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/i-MX-8M-Family-DDR-Tool-Release/ta-p/110...

Also recommended to use latest nxp uboot/linux described on

https://www.nxp.com/design/software/embedded-software/i-mx-software/embedded-linux-for-i-mx-applicat...

 

Best regards
igor

0 Kudos
Reply

3,003 Views
shamiullah
Contributor III

Hi igor,

Thanks for the suggestion.

Followed MSCALE ddr tool user guide and generated custom uboot binary. 

ddr stress test gets success, but when i try to boot the custom board with newly generated uboot, it hangs at 

starting kernel ......

after this print i can see a garbage is printing on the console.

Please find the attachment for boot log

 

Thanks 

shami

0 Kudos
Reply