sabresd uboot SPL

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

sabresd uboot SPL

3,784 Views
leonardoprates
Contributor III

I have enabled SPL_BUILD in uboot and it compiles ok, I configure DDR parameters in sabresd.c file just like my DCD (that works) but SPL doesn't boot ( at least I can't see any log in console). My questions are:

1. Printf works in SPL to generate log? 

2. How SPL finds uboot.

3. I have to write to SdCard SPL file and uboot.img? Which seek I have to use in DD?

4. Uboot from freescale works SPL only enabling SPL_BUILD?

0 Kudos
Reply
4 Replies

2,859 Views
igorpadykov
NXP Employee
NXP Employee

Hi Leonardo

nxp uboot does not use spl

uboot-imx.git - Freescale i.MX u-boot Tree 

one can post this on uboot mail list

U-Boot Info Page 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

2,859 Views
leonardoprates
Contributor III

Hi Igor, thanks for your answer. Only a doubt in the sabresd file http://git.freescale.com/git/cgit.cgi/imx/uboot-imx.git/tree/board/freescale/mx6sabresd/mx6sabresd.c... 

At line 374 and 1320 there are configs for SPL, this not work?

0 Kudos
Reply

2,859 Views
mach
Contributor I

Hello Leonardo,

I've met the question as you too.(https://community.nxp.com/message/864563 ) Do you solve it? If yes, could you show me some details? Thanks.

Best wishes,

Mc

0 Kudos
Reply

2,859 Views
igorpadykov
NXP Employee
NXP Employee

please check

https://community.freescale.com/message/402940#402940

this option is not used in nxp uboot, though it is present in codes.

One can also post this to meta-fsl-arm mailing list, so that someone familiar with it

could try to assist you.

https://lists.yoctoproject.org/listinfo/meta-freescale

Best regards
igor

0 Kudos
Reply