sabresd imx7 board schematics

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

sabresd imx7 board schematics

跳至解决方案
8,296 次查看
adnanali
Contributor III

I need schematics for both sabresd board and epdc panel.

i.MX 7Dual SABRE Board|NXP

Can you please refer me from where can I download them if they are available publicly. If they are not available to public kindly let me know whether Max17135 PMIC chip is connected on sabre board or the epdc panel.

Regards

标签 (4)
1 解答
4,843 次查看
igorpadykov
NXP Employee
NXP Employee

Hi adnan

please check

Schematics (2)

Design files for i.MX 7Dual (REV D)

Design files, including hardware schematics, Gerbers, and OrCAD files for i.MX 7Dual (REV D)

http://www.nxp.com/products/microcontrollers-and-processors/arm-processors/i.mx-applications-process...

Max17135 PMIC chip is located on IMXEBOOKDC4 board, one can try to enter service

request for obtaining it (note NDA may be needed).

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

9 回复数
4,843 次查看
elenarimoldi
Contributor II

I am having an issue with loading images on the EPD - any idea where this error might come from:

IMG_3037.JPG

0 项奖励
回复
4,843 次查看
marcocavallini
Contributor V

Could you please point me to the iMX7DSABRESD schematics in PDF format ?

0 项奖励
回复
4,843 次查看
indirokanovic
Contributor II

marcocavallini‌ here it is. Design files, including hardware schematics, Gerbers, and OrCAD files for i.MX 7Dual

I meant to attach pdf directly but you will need to agree to NDA and download it yourself.

0 项奖励
回复
4,844 次查看
igorpadykov
NXP Employee
NXP Employee

Hi adnan

please check

Schematics (2)

Design files for i.MX 7Dual (REV D)

Design files, including hardware schematics, Gerbers, and OrCAD files for i.MX 7Dual (REV D)

http://www.nxp.com/products/microcontrollers-and-processors/arm-processors/i.mx-applications-process...

Max17135 PMIC chip is located on IMXEBOOKDC4 board, one can try to enter service

request for obtaining it (note NDA may be needed).

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

4,843 次查看
elenarimoldi
Contributor II

Hi igorpadykov,

I have the same problem of Jonathan, I am looking for the schematics of i.MX7 Dual board, but the link you mentioned does not seem to contain this information. Any idea on where else I can look at for this information?

Thanks!

0 项奖励
回复
4,843 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Elena

I checked link, below is schematics of i.MX7 Dual board

pastedImage_1.jpg

Best regards
igor

4,843 次查看
elenarimoldi
Contributor II

thanks igorpadykov! I could find the schematics.

I now have another issue - I am trying to find the waveform for the specific epdc that I am using - a 13.3" E-Ink (model ED133UT2). I cannot find the waveform in the /lib/firmware/imx/epdc directory (although I did find the waveform for smaller displays, especially the 6inches ones). Do you have any idea where I might find this information or how I could generate the waveform specific for this display?

0 项奖励
回复
4,843 次查看
karolmlynczak
Contributor II

I also join in the request to find waveform to ED133UT2 screen. The file witch waveform should be called epdc_ED133UT2.fw or epdc_E133UT2.fw.ihex.

4,843 次查看
jhtate1
Contributor I

Hello igorpadykov,

 

Do you have these same schematics in Altium?

Thank you.

0 项奖励
回复