running gstreamer without a v4l2 device on ARM dual-core

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

running gstreamer without a v4l2 device on ARM dual-core

1,234 Views
mihaitaivascu
Contributor III

Hello,

    I would like to run gstreamer to create a video streaming application but I do not use a v4l2 camera or other device.

Instead I have running  a FreeRTOS on the other core and there the frames are copied in the memory. Because the camera is controlled and configured from that core.

    I have a shared memory pool between the 2 cores and would like to fetch the frames from the memory using a char device driver and then have a gstreamer app running on top of it. The first core runs an embedded Linux and the second a FreeRTOS.

   Is this a feasible scenario?

   I have came across this v4l2 plugin for mem-to-mem transfers:

GitHub - igel-oss/v4l-gst: A v4l plugin to bridge V4L2 APIs and GStreamer 

   Does anybody has experience with this approach?

Thanks,

      Mihaita

Labels (1)
0 Kudos
Reply
0 Replies