running A7 and M4 in parallel in IMX7 Dual SabreSD board

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

running A7 and M4 in parallel in IMX7 Dual SabreSD board

580 Views
ehsanurrub
Contributor I

hi Gregor

I have IMX7 DUAL SABRE SD board.

I am trying to run A7  core and M4 core in parallel , however i am not able to achieve this Task.

In other words i am trying to run Linux on A7 and FreeRtos in M4 in Parallel , but i am not able to achieve this Task

Can you please help me out with this issue ?

Labels (1)
0 Kudos
1 Reply

374 Views
jamesbone
NXP TechSupport
NXP TechSupport

Hello Ehsan,

You first need to create a  SD card with the Linux BSP image, please see the following document,

Preparing Linux bootable SD card for i.MX6UL  

Once you have the Linux you are going to finda package that contains the  FREERtos BSP for the M4 and you would be able to install it jut like another software package in Linux.


Have a great day,
TIC

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos