rt3070 wifi soft ap imx53 android

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

rt3070 wifi soft ap imx53 android

Jump to solution
3,218 Views
ff
Contributor II

hi everone

   recently i was working on a usb wifi ,rt3070,

when i start the wifi soft ap function,i received an error;

here is the log

I/dispd   ( 2080): path:/module/rtutil3070ap

I/dispd   ( 2080): path:/module/rt3070ap

I/dispd   ( 2080): path:/module/rtnet3070ap

D/Tethering( 2116): sendTetherStateChangedBroadcast 1, 0, 0

D/Tethering( 2116): interfaceAdded :ra0

I/dispd   ( 2080): path:/devices/virtual/net/ra0

I/dispd   ( 2080): path:/bus/usb/drivers/rt2870

D/CommandListener( 2079): Setting iface cfg

D/Tethering( 2116): Tethering ra0

D/Tethering( 2116): InitialState.processMessage what=2

D/NetworkManagmentService( 2116): rsp <213 00:00:00:00:00:00 0.0.0.0 0.0.0.0 [down broadcast multicast]>

D/NetworkManagmentService( 2116): flags <[down broadcast multicast]>

D/Tethering( 2116): sendTetherStateChangedBroadcast 0, 0, 0

D/Tethering( 2116): Tethered ra0

D/Tethering( 2116): sendTetherStateChangedBroadcast 0, 1, 0

D/Tethering( 2116): MasterInitialState.processMessage what=1

D/Tethering( 2116): Tether Mode requested by ra0 - TetheredState - Tethered - lastError =0

D/NetworkManagmentService( 2116): rsp <213 00:00:00:00:00:00 0.0.0.0 0.0.0.0 [down broadcast multicast]>

D/NetworkManagmentService( 2116): flags <[down broadcast multicast]>

D/NetworkManagmentService( 2116): rsp <213 00:00:00:00:00:00 192.168.43.1 255.255.255.0 [down broadcast multicast]>

D/NetworkManagmentService( 2116): flags <[down broadcast multicast]>

D/Tethering( 2116): chooseUpstreamType(false),  dunRequired =false, iface=null

D/Tethering( 2116): notifying tethered with iface =null

D/TetherController( 2079): Setting IP forward enable = 1

D/TetherController( 2079): Starting tethering services

D/TetherController( 2079): Tethering services running

D/TetherController( 2079): setDnsForwarders(0 = '8.8.8.8')

D/TetherController( 2079): setDnsForwarders(1 = '4.2.2.2')

D/TetherController( 2079): Sending update msg to dnsmasq [update_dns:8.8.8.8:4.2.2.2]

D/Tethering( 2116): TetheredState.processMessage what=12

I/dnsmasq ( 2417): started, version 2.51 cachesize 150

I/dnsmasq ( 2417): compile time options: no-IPv6 GNU-getopt no-DBus no-I18N DHCP no-scripts no-TFTP

W/dnsmasq ( 2417): warning: no upstream servers configured

I/dnsmasq ( 2417): DHCP, IP range 192.168.43.2 -- 192.168.43.254, lease time 1h

I/dnsmasq ( 2417): DHCP, IP range 192.168.42.2 -- 192.168.42.254, lease time 1h

I/dnsmasq ( 2417): read /etc/hosts - 1 addresses

I/dnsmasq ( 2417): using nameserver 4.2.2.2#53

I/dnsmasq ( 2417): using nameserver 8.8.8.8#53

D/dalvikvm( 2116): GC_CONCURRENT freed 1002K, 46% free 4374K/8007K, external 2765K/3965K, paused 4ms+15ms

E/SoftapController( 2079): Softap driver stop - function not supported

E/WifiService( 2116): Exception in startAccessPoint()

int SoftapController::getPrivFuncNum(char *iface, const char *fname) {
    struct iwreq wrq;
    struct iw_priv_args *priv_ptr;
    int i, ret;

    strncpy(wrq.ifr_name, iface, sizeof(wrq.ifr_name));
    wrq.u.data.pointer = mBuf;
    wrq.u.data.length = sizeof(mBuf) / sizeof(struct iw_priv_args);
    wrq.u.data.flags = 0;
    if ((ret = ioctl(mSock, SIOCGIWPRIV, &wrq)) < 0) {
        LOGE("SIOCGIPRIV failed: %d", ret);
        return ret;
    }
    priv_ptr = (struct iw_priv_args *)wrq.u.data.pointer;
    for(i=0;(i < wrq.u.data.length);i++) {
        if (strcmp(priv_ptr[i].name, fname) == 0)
            return priv_ptr[i].cmd;
    }
    return -1;
}

i can not figure it out,is there somebody familiar with android  wifi soft ap,please give me some advice

thanks inadvance

the file is the whole log

 

in this function  it return an error

    fnum = getPrivFuncNum(iface, "START");

 

 

Original Attachment has been moved to: untitle.txt.zip

Labels (2)
0 Kudos
Reply
1 Solution
2,050 Views
max_tsai
NXP Employee
NXP Employee

hi,

According to your log, it seems iwreq struct is not filled well, or your wireless driver doesn't provide "START"/"STOP" commands within Wireless Extention for Android. You can check athero wireless driver of default BSP,

--

//"system/wlan/atheros/AR6kSDK.build_3.1_RC.563/host/os/linux/ar6000_android.c"

370 int android_ioctl_siwpriv(struct net_device *dev,

371               struct iw_request_info *__info,

372               struct iw_point *data, char *__extra)

373 {

585     } else if (strcasecmp(cmd, "START")==0 || strcasecmp(cmd, "STOP")==0) {


View solution in original post

0 Kudos
Reply
3 Replies
2,050 Views
YixingKong
Senior Contributor IV

ff, if your question has been answered, please click Correc Answer, so that we may close the DI.

Thanks,

Yixing

0 Kudos
Reply
2,051 Views
max_tsai
NXP Employee
NXP Employee

hi,

According to your log, it seems iwreq struct is not filled well, or your wireless driver doesn't provide "START"/"STOP" commands within Wireless Extention for Android. You can check athero wireless driver of default BSP,

--

//"system/wlan/atheros/AR6kSDK.build_3.1_RC.563/host/os/linux/ar6000_android.c"

370 int android_ioctl_siwpriv(struct net_device *dev,

371               struct iw_request_info *__info,

372               struct iw_point *data, char *__extra)

373 {

585     } else if (strcasecmp(cmd, "START")==0 || strcasecmp(cmd, "STOP")==0) {


0 Kudos
Reply
2,050 Views
ff
Contributor II


hi  MaxTsai

yes it's because  my wireless driver doesn't provide "START"/"STOP" commands within Wireless Extention for Android.

ths

0 Kudos
Reply