rt linux for imx6ullevk

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

rt linux for imx6ullevk

888 Views
rajesh-d
Contributor I

hi

im using imx6ull , where i need to enable prmeept_rt patch, i have enabled 

--->General setup

               -->(X) Fully Preemptible Kernel (Real-Time) 

in  Linux kernel 5.4.3 by using patch-5.4.3-rt1.patch.xz and created kernel image and i tried to boot the board with rootfs build (poky branch is kirkstone) using core-image-minimal image recipe it was not providing me root access ,

So i tried to build another rootfs (poky branch is kirkstone) using core-image-rt-sdk image recipe in yocto toster it is showing error. as

Nothing PROVIDES 'core-image-rt-sdk'

core-image-rt-sdk was skiped : Set PREFERRED_PROVIDER_virtual/kernel to linux-yocto-rt to enable it

how to build rootfs using core-image-rt-sdk image recipe .

 

0 Kudos
Reply
0 Replies