rpmdb: --force-debian: unknown option error using LTIB 9.1.1 on Ubuntu 11.10

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

rpmdb: --force-debian: unknown option error using LTIB 9.1.1 on Ubuntu 11.10

3,602 Views
AdCmo
Contributor III

When running LTIB 9.1.1 on Ubuntu 11.10

I get the following error when I run:

 

./ltib -m config  OR if I run ./ltib

 

Here is the error in /opt/freescale/ltib/host_config.log

 

rpmdb: --force-debian: unknown option
Died at ./ltib line 2346.
traceback:
 main::setup_rpmdb:2346
  main::check_rpm_setup:2409
   main::host_checks:1429
    main:542

 

I looked at the suggestions here:

http://forums.freescale.com/t5/i-MX-Microprocessors/iMX25-install-ltib/td-p/49730

and here:

http://forums.freescale.com/t5/i-MX-Microprocessors/Ltib/m-p/57697

 

None of them seem to work for me,

Any clues?

Ad.

----------------------------------------------------

Tags (1)
0 Kudos
Reply
10 Replies

2,416 Views
KrishnaPavan
Contributor II

Hi Katerina,

                 If you have managed to pass this error, then, can you open a new thread with your current issue, attaching the config_log, by posting it in a respective Group, say for example, if you are using i.MX53, then post in the respective group in imxcommunity.org.

 

Also post here, hoe you got past of your previous error, as it would be helpful for other members in the imxcommunity.org.

Regards  ::  Krishna Pavan

0 Kudos
Reply

2,416 Views
KaterinaKaminsk
Contributor I

I managed to pass this error, but get another:

 

make[1]: *** wait: No child processes.  Stop.make[1]: *** Waiting for unfinished jobs....make[1]: *** wait: No child processes.  Stop.make: *** wait: No child processes.  Stop.make: *** Waiting for unfinished jobs....make: *** wait: No child processes.  Stop.make[2]: *** [os_alloc.lo] Error 1

Krishna Pavan said:

0 Kudos
Reply

2,416 Views
KrishnaPavan
Contributor II
0 Kudos
Reply

2,416 Views
KaterinaKaminsk
Contributor I

Lubuntu 12.04 x32, IMX.508, LTIB 9.1.1 (I guess, was included to reader SDK)

Krishna Pavan said:

Hi Katerina,

 

Just list out the above mentioned,

OS Version, Board You are using, Bootloader used.

 

Try this link http://www.imxdev.org/wiki/index.php?title=FAQ.

It seems, you are using a different, unsupported version of some package......

 

Regards   :::   Krishna Pavan

0 Kudos
Reply

2,416 Views
AdCmo
Contributor III

I was able to get past this issue by applying the patch I mentioned above.

i.e. manually modifying those diff lines above.

 

Ad

------------------------------

0 Kudos
Reply

2,416 Views
AdCmo
Contributor III

All,

The problem was solved in the main line latest LTIB.

The trick now is to integrate it into the existing 9.1.1 LTIB version supplied by Freescale.

Here is the patch on the mailine LTIB site.

http://cvs.savannah.gnu.org/viewvc/ltib/ltib?root=ltib&r1=1.76&r2=1.77

 

Ad.

--------------------------

0 Kudos
Reply

2,416 Views
KrishnaPavan
Contributor II

Hi Katerina,

 

Just list out the above mentioned,

OS Version, Board You are using, Bootloader used.

 

Try this link http://www.imxdev.org/wiki/index.php?title=FAQ.

It seems, you are using a different, unsupported version of some package......

 

Regards   :::   Krishna Pavan

0 Kudos
Reply

2,416 Views
KaterinaKaminsk
Contributor I

nothing change. still get error.

rpmdb: --force-debian: unknown option

Died at ./ltib line 2340.

traceback: main::setup_rpmdb:2340 

               main::check_rpm_setup:2403   

               main::host_checks:1423   

               main:542


Krishna Pavan said:

Hi,

For the time being go to this link and try to find out some solution

http://www.imxdev.org/wiki/index.php?title=All_Boards_LTIB

just list out what is the OS on which you are working, along with other details like, the board,the boot-loader you are using, etc.

 

Regards Krishna Pavan

0 Kudos
Reply

2,416 Views
KrishnaPavan
Contributor II

Hi,

For the time being go to this link and try to find out some solution

http://www.imxdev.org/wiki/index.php?title=All_Boards_LTIB

just list out what is the OS on which you are working, along with other details like, the board,the boot-loader you are using, etc.

 

Regards Krishna Pavan

0 Kudos
Reply

2,416 Views
KaterinaKaminsk
Contributor I

I have the very same problem! Can anyone give any clue? I'm actually newbie in freescale controllers, so can't figure this out myself

0 Kudos
Reply