restarting rtsp stream leaves system in bad state

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

restarting rtsp stream leaves system in bad state

2,779件の閲覧回数
alokkumar
Contributor III

Hi,

I have been experiencing if I kill already running gsteamer RTSP stream/playing video, it leaves earlier image on display and when running again without rebooting the board, it is likely that it would not work (you will not see the stream on display).

My question is, what is best way to restart a video/stream without rebooting the board ?

I am using imx6Q Nitrogen board.

Thanks in advance for help.

Alok

ラベル(3)
0 件の賞賛
返信
4 返答(返信)

2,556件の閲覧回数
LeonardoSandova
Specialist I

Hi Alok,

could you post the pipeline you are running? is your video playback on main screen (/dev/video17)?

Leo

0 件の賞賛
返信

2,556件の閲覧回数
alokkumar
Contributor III

Hi Leo,

Thanks for the reply and you kind attention for the issue.

This is the pipe line I am using (Actually I am using C equivalent of this in program.

gst-launch rtspsrc location= rtsp://10.10.0.56/vbStream1S1 name =demux ! queue max-size-buffers=0 max-size-time=0  ! rtph264depay ! capsfilter caps="video/x-h264,width=1920,height=1080,framerate=(fraction)60/1" ! vpudec ! queue max-size-buffers=0 max-size-time=0 ! mfw_v4lsink sync=false demux. ! rtpmp4gdepay ! beepdec ! queue max-size-buffers=0 max-size-time=0  ! 'audio/x-raw-int, channels=2' ! alsasink device='hw:1,0' sync=false

When I kill this program with control C, I see display left with last still image and next time play does not work sometimes.

As per our project requirement  we will be changing the display stream/video/images at run time, so I am struggling to find out how can I have robust code.

Thanks

Alok

0 件の賞賛
返信

2,557件の閲覧回数
alokkumar
Contributor III

I forgot to mention, My display is divided with multiple widgets and one of the widget is RTSP stream/Video.

0 件の賞賛
返信

2,557件の閲覧回数
timothybean
Contributor IV

I don't know if you have figured this out yet. But on your mfw_v4lsink use device=/dev/video17 instead of nothing. When you leave it blank you are going to video16 output which is RGB output. After stopping, it leaves last frame there. Using video17 is the video overlay and that will not happen when you stop. It will go blank instead, OR, show the RGB layer underneath if you had something on it.

Tim