resource partition to share GPIO3 between A35 and M4

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

resource partition to share GPIO3 between A35 and M4

1,419件の閲覧回数
xiaokaoy
Contributor I

Hello.

I'm using i.MX8DualX. Some GPIO3 pins will be accessed by A35 and the other GPIO3 pins by M4. My wrote some code in board_system_config for that like this

 

BRD_ERR(rm_assign_resource(pt_boot, pt_sh, SC_R_GPIO_3));
BRD_ERR(rm_set_peripheral_permissions(pt_sh,
SC_R_GPIO_3, pt_boot, SC_RM_PERM_FULL));
BRD_ERR(rm_set_peripheral_permissions(pt_sh,
SC_R_GPIO_3, pt_m4_0, SC_RM_PERM_FULL));

 

I also moved those pads for M4 to the M4 partition:

BRD_ERR(rm_set_pad_movable(pt_boot, SC_P_QSPI0B_SCLK,
SC_P_COMP_CTL_GPIO_1V8_3V3_QSPI0B, SC_TRUE));

 

but it doesn't work.

0 件の賞賛
返信
3 返答(返信)

1,407件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi xiaokaoy

 

according to description below:

"Pads and resources CANNOT BE SHARED there is no mechanism to protect the
pads and resources from contention, if access to a resource is required by multiple
partitions a virtual resource needs to be created, in this way the partition that requires
access asks the partition that owns the resource to configure/use
the resource on its behalf. See the VIRT_I2C example on the Linux BSP. "

https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/System-Controller-Firmware-101-Resource-...

 

https://source.codeaurora.org/external/imx/linux-imx/tree/drivers/i2c/busses/i2c-rpmsg-imx.c?h=imx_5...

 

Best regards
igor

0 件の賞賛
返信

1,382件の閲覧回数
xiaokaoy
Contributor I

Thanks for your reply.

Do you mean that it is impossible to share GPIO3 even if A35 and M4 only access their respective groups of GPIO3 pins? e.g. A35 only accesses GPIO3_IO01/02/03 while M4 only accesses GPIO3_IO04/05/06? 

0 件の賞賛
返信

1,363件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi xiaokaoy

 

unfortunately such examples are not available.

 

Best regards
igor

0 件の賞賛
返信