reset key can't reboot system

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

reset key can't reboot system

645 次查看
yan2anfei
Contributor III

hi ,

I have a custom board base on imx6sl, 

when the system is booting  , press reset button,system can reboot, but if the system boot complete,press reset button, the system do anything,Looks like  crash. 

Has some people encountered this situation and how to solve?

thanks.

标签 (2)
0 项奖励
1 回复

491 次查看
igorpadykov
NXP Employee
NXP Employee

Hi yan2

please refer to attached Release Notes

pastedImage_1.jpg

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励