reset key can't reboot system

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

reset key can't reboot system

647件の閲覧回数
yan2anfei
Contributor III

hi ,

I have a custom board base on imx6sl, 

when the system is booting  , press reset button,system can reboot, but if the system boot complete,press reset button, the system do anything,Looks like  crash. 

Has some people encountered this situation and how to solve?

thanks.

ラベル(2)
0 件の賞賛
1 返信

493件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi yan2

please refer to attached Release Notes

pastedImage_1.jpg

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛