repo init error

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

repo init error

11,461件の閲覧回数
shamiullah
Contributor III

Hello @all,

when i running repo init command i am facing the following issues for android 10 source.

ERROR:

-----------------------------------------------------------------

Start fetching the source for android build
Setting REL_PACKAGE_DIR to /home/prasanth/shammi/android10/imx-android-10.0.0_2.0.0
Setting WORKSPACE to /home/prasanth/shammi/android10/imx-android-10.0.0_2.0.0
Setting android_builddir to /home/prasanth/shammi/android10/imx-android-10.0.0_2.0.0/android_build
Downloading Repo source from https://gerrit.googlesource.com/git-repo
Traceback (most recent call last):
File "/home/prasanth/shammi/android10/imx-android-10.0.0_2.0.0/android_build/.repo/repo/main.py", line 42, in <module>
from git_config import RepoConfig
File "/home/prasanth/shammi/android10/imx-android-10.0.0_2.0.0/android_build/.repo/repo/git_config.py", line 774
self._Set(f'superproject.{key}', value)
^
SyntaxError: invalid syntax
---------------------------------------------------
-----Repo Init failure
---------------------------------------------------
./imx_android_setup-ALPHA1.sh: line 66: return: can only `return' from a function or sourced script
Traceback (most recent call last):
File "/home/prasanth/shammi/android10/imx-android-10.0.0_2.0.0/android_build/.repo/repo/main.py", line 42, in <module>
from git_config import RepoConfig
File "/home/prasanth/shammi/android10/imx-android-10.0.0_2.0.0/android_build/.repo/repo/git_config.py", line 774
self._Set(f'superproject.{key}', value)
^
SyntaxError: invalid syntax
Try repo sync 1 time(s)
Traceback (most recent call last):
File "/home/prasanth/shammi/android10/imx-android-10.0.0_2.0.0/android_build/.repo/repo/main.py", line 42, in <module>
from git_config import RepoConfig
File "/home/prasanth/shammi/android10/imx-android-10.0.0_2.0.0/android_build/.repo/repo/git_config.py", line 774
self._Set(f'superproject.{key}', value)
^
SyntaxError: invalid syntax
Try repo sync 2 time(s)
Traceback (most recent call last):
File "/home/prasanth/shammi/android10/imx-android-10.0.0_2.0.0/android_build/.repo/repo/main.py", line 42, in <module>
from git_config import RepoConfig
File "/home/prasanth/shammi/android10/imx-android-10.0.0_2.0.0/android_build/.repo/repo/git_config.py", line 774
self._Set(f'superproject.{key}', value)
^
SyntaxError: invalid syntax
Try repo sync 3 time(s)
Traceback (most recent call last):
File "/home/prasanth/shammi/android10/imx-android-10.0.0_2.0.0/android_build/.repo/repo/main.py", line 42, in <module>
from git_config import RepoConfig
File "/home/prasanth/shammi/android10/imx-android-10.0.0_2.0.0/android_build/.repo/repo/git_config.py", line 774
self._Set(f'superproject.{key}', value)
^
SyntaxError: invalid syntax
Traceback (most recent call last):
File "/home/prasanth/shammi/android10/imx-android-10.0.0_2.0.0/android_build/.repo/repo/main.py", line 42, in <module>
from git_config import RepoConfig
File "/home/prasanth/shammi/android10/imx-android-10.0.0_2.0.0/android_build/.repo/repo/git_config.py", line 774
self._Set(f'superproject.{key}', value)
^
SyntaxError: invalid syntax
---------------------------------------------------
------Repo sync failure
---------------------------------------------------
./imx_android_setup-ALPHA1.sh: line 88: return: can only `return' from a function or sourced script
fatal: can't open patch '/home/prasanth/shammi/android10/imx-android-10.0.0_2.0.0/android_build/device/fsl/imx8m/phyboard_polis/patch/0001-imx8mm_bl31_setup-allow-uart4-from-A53-processor.patch': No such file or directory
fatal: can't open patch '/home/prasanth/shammi/android10/imx-android-10.0.0_2.0.0/android_build/device/fsl/imx8m/phyboard_polis/patch/0001-Parsing-the-devicetree-name.patch': No such file or directory
Android source is ready for the build

-----------------------------------------------------------------

 

 

With Regards,

Shamiullah

ラベル(2)
0 件の賞賛
返信
6 返答(返信)

11,441件の閲覧回数
Zhiming_Liu
NXP TechSupport
NXP TechSupport

@shamiullah 

 

It seems your git doesn't have a correct config.Can you attach your all commands?

0 件の賞賛
返信

11,431件の閲覧回数
shamiullah
Contributor III

Hi @Zhiming_Liu 

The above issue got resolved by downlaoding gitconfig but i am facing other issue

Below are the logs:

-------------------------------------------------------------------------------------------------------------------------------------------prasanth@phytec1:~/shammi/android10/imx-android-10.0.0_2.0.0/android_build$ repo init -u https://stash.phytec.com/scm/asdk/platform-manifests.git -b imx-android-10 -m ALPHA1.xml
prasanth@phytec1:~/shammi/android10/imx-android-10.0.0_2.0.0/android_build$ /usr/bin/repo init -u https://stash.phytec.com/scm/asdk/platform-manifests.git -b imx-android-10 -m ALPHA1.xml
File "/home/prasanth/shammi/android10/imx-android-10.0.0_2.0.0/android_build/.repo/repo/main.py", line 79
file=sys.stderr)
^
SyntaxError: invalid syntax
prasanth@phytec1:~/shammi/android10/imx-android-10.0.0_2.0.0/android_build$ ~/bin/repo init -u https://stash.phytec.com/scm/asdk/platform-manifests.git -b imx-android-10 -m ALPHA1.xml

-----------------------------------------------------------------------------------------------------------

When i use repo binary downloaded by the curl commands i am getting any error but it is taking less time to execute the command as shown above

When i use repo binary from /usr/bin/ , i am facing the following issue as shown below

File "/home/prasanth/shammi/android10/imx-android-10.0.0_2.0.0/.repo/repo/main.py", line 79
file=sys.stderr)
^
SyntaxError: invalid syntax

 

I downloaded the repo by using the below commands

$ mkdir ~/bin
$ curl https://storage.googleapis.com/git-repo-downloads/repo > ~/bin/repo
$ chmod a+x ~/bin/repo
$ export PATH=${PATH}:~/bin

 

Please let me know

Thanks & Regards

Shamiullah

0 件の賞賛
返信

7,753件の閲覧回数
sbhattad
Contributor I

Hello @shamiullah ,

Facing issue while repo init regarding git config. Kindly help me to resolve.

ivi@Jenkins:~/AndroidEmulator$ cat ~/.gitconfig
[user]
email = shraddhabhattad15@gmail.com
name = shraddhabhattad15
ivi@Jenkins:~/AndroidEmulator$ python3 ~/bin/repo init -u https://android.googlesource.com/platform/manifest -b android-10.0.0_r47
Traceback (most recent call last):
File "/home/ivi/AndroidEmulator/.repo/repo/main.py", line 42, in <module>
from git_config import RepoConfig
File "/home/ivi/AndroidEmulator/.repo/repo/git_config.py", line 774
self._Set(f'superproject.{key}', value)
^
SyntaxError: invalid syntax

0 件の賞賛
返信

6,313件の閲覧回数
cuiliu
NXP Employee
NXP Employee

Facing the same issue. Have resolved it. 

If you still don't know how to solve the issue, maybe you can try this:

It is not related to git_config but to the version of python. Maybe you curl repo with python2 and thus the .repo in you Android folder is false. You can do this to fix it:

1, change your python version

$ sudo update-alternatives --config python 

then enter number of python3

$ python --version

if display python3***,is right

 

2,remove your repo

$ which repo

$ sudo rm -rf /home/***/bin/repo

$ curl https://storage.googleapis.com/git-repo-downloads/repo > ~/bin/repo
$ chmod a+x ~/bin/repo
$ export PATH=${PATH}:~/bin

 

3,remove .repo in android folder

$ sudo rm -rf  android_forder/.repo

 

3,At last,you can repo init successfully

0 件の賞賛
返信

11,332件の閲覧回数
IgorKorolyuk
Contributor I

Hello, @shamiullah .

I'm facing the same issue.
Can you please add details on "downlaoding gitconfig", I don't seem to understand what it is exactly and the way it helps.

Thank you.

0 件の賞賛
返信

11,400件の閲覧回数
Zhiming_Liu
NXP TechSupport
NXP TechSupport

Do you input correct xml?Your input xml name is (imx-android-10 -m ALPHA1.xml), it contains spaces.

0 件の賞賛
返信