reboot操作后emmc损坏

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

reboot操作后emmc损坏

1,787 Views
wujb18
Contributor I

        状态情况,手里有两张在调试的板子,已经运行调试两周左右,软件工程师在某一次reboot操作后,板子不能启动了,没有任何打印信息,这时断电检查发现,EMMC的一路电源被击穿,对地短路。我对比了电路,没有发现异常,重新更换一片可以正常运行。对电源做了上百次的监测,没有发现异常。

         目前想查找真正的原因是什么?操作系统是LINUX3.0.35。IMX6原版设计EMMC采用SDIN5C2-8G_NRND, 现在设计采用的是SM661GE8BAA,通过 这段时间的查找问题发现,了解到三星在手机产品之前,出现的”字库门“事件,这才让我知道,EMMC问题的可能性,以前一直怀疑硬件的问题,没有从软件角度考虑。看了三星事件后,对于网上说是由于软件部分命令和EMMC驱动、开关机的操作方式可能对其损坏,没有人对这个比较全面详细剖析。请你们分析一下我板子(IMX6Q6A+SM661GE8BAA)可能导致的原因。是否跟三星字库门有对比性。

         还有一问题,IMX6Q6A的接口是EMMC4.4.  SM661GE8BAA是EMMC4.5,我查看一下驱动,是否需要补丁,谢谢!

Labels (1)
0 Kudos
1 Reply

774 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

Hi,

About your above question my colleague has given reply to you in our salesforce system, please have a check. And about the emmc version question you can refer to the thread in our community:EMMC 5.0 and EMMC 5.1 work on i.MX6 .
Have a great day,
Rita

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos